Skip to main content
Associate III
May 16, 2025 5:37 AM UTC
Question

Deploying the image classification model on the STM32N6570-DK got stuck, seeking help.

Hello everyone,

I followed the tutorial below to deploy, and an error occurred when executing python stm32ai_main.py at the end. The window log is as follows. Can anyone help me figure out what happened?

https://github.com/STMicroelectronics/stm32ai-modelzoo-services/blob/main/image_classification/deployment/README_STM32N6.md

 

LOAD ERROR: WindowsPath('E:/07_Stm32/stm32N657/stm32ai-modelzoo-main/stm32ai-modelzoo-services-main/stm32ai-modelzoo-services/image_classification/src/deployment_outputs/2025_05_16_13_00_27/network.h') and WindowsPath('E:/07_Stm32/stm32N657/stm32ai-modelzoo-main/stm32ai-modelzoo-services-main/stm32ai-modelzoo-services/image_classification/src/deployment_outputs/2025_05_16_13_00_27/network.h') are the same file
Error executing job with overrides: []
Traceback (most recent call last):
File "E:\07_Stm32\stm32N657\stm32ai-modelzoo-main\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services\image_classification\src\stm32ai_main.py", line 421, in <module>
main()
File "D:\26_anaconda3\envs\n61\lib\site-packages\hydra\main.py", line 94, in decorated_main
_run_hydra(
File "D:\26_anaconda3\envs\n61\lib\site-packages\hydra\_internal\utils.py", line 394, in _run_hydra
_run_app(
File "D:\26_anaconda3\envs\n61\lib\site-packages\hydra\_internal\utils.py", line 457, in _run_app
run_and_report(
File "D:\26_anaconda3\envs\n61\lib\site-packages\hydra\_internal\utils.py", line 223, in run_and_report
raise ex
File "D:\26_anaconda3\envs\n61\lib\site-packages\hydra\_internal\utils.py", line 220, in run_and_report
return func()
File "D:\26_anaconda3\envs\n61\lib\site-packages\hydra\_internal\utils.py", line 458, in <lambda>
lambda: hydra.run(
File "D:\26_anaconda3\envs\n61\lib\site-packages\clearml\binding\hydra_bind.py", line 91, in _patched_hydra_run
return PatchHydra._original_hydra_run(self, config_name, task_function, overrides, *args, **kwargs)
File "D:\26_anaconda3\envs\n61\lib\site-packages\hydra\_internal\hydra.py", line 132, in run
_ = ret.return_value
File "D:\26_anaconda3\envs\n61\lib\site-packages\hydra\core\utils.py", line 260, in return_value
raise self._return_value
File "D:\26_anaconda3\envs\n61\lib\site-packages\hydra\core\utils.py", line 186, in run_job
ret.return_value = task_function(task_cfg)
File "D:\26_anaconda3\envs\n61\lib\site-packages\clearml\binding\hydra_bind.py", line 230, in _patched_task_function
return task_function(a_config, *a_args, **a_kwargs)
File "E:\07_Stm32\stm32N657\stm32ai-modelzoo-main\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services\image_classification\src\stm32ai_main.py", line 407, in main
process_mode(mode=mode, configs=cfg, train_ds=train_ds, valid_ds=valid_ds, quantization_ds=quantization_ds,
File "E:\07_Stm32\stm32N657\stm32ai-modelzoo-main\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services\image_classification\src\stm32ai_main.py", line 302, in process_mode
deploy(cfg=configs)
File "E:\07_Stm32\stm32N657\stm32ai-modelzoo-main\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services\image_classification\src\../deployment\deploy.py", line 90, in deploy
stm32ai_deploy_stm32n6(target=board, stlink_serial_number=stlink_serial_number, stm32ai_version=stm32ai_version, c_project_path=c_project_path,
File "E:\07_Stm32\stm32N657\stm32ai-modelzoo-main\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services\image_classification\src\../../common/deployment\common_deploy.py", line 469, in stm32ai_deploy_stm32n6
stmaic_local_call(session)
File "E:\07_Stm32\stm32N657\stm32ai-modelzoo-main\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services\image_classification\src\../../common/deployment\common_deploy.py", line 443, in stmaic_local_call
stmaic.compile(session=session, options=opt, target=session._board_config)
File "E:\07_Stm32\stm32N657\stm32ai-modelzoo-main\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services\image_classification\src\../../common\stm32ai_local\compile.py", line 208, in cmd_compile
raise Exception('Error during compilation')
Exception: Error during compilation

This topic has been closed for replies.

2 replies

GRATT.2
ST Employee
May 16, 2025 2:44 PM UTC

Hello, 

A new release is on its way and will be published next week. Thus, we won't address these bugs. 

Guillaume

GHORT.1
ST Employee
May 20, 2025 1:57 PM UTC

The new version of the model zoo is available:

STMicroelectronics/stm32ai-modelzoo-services at v3.1.0

We released the STM32N6 code in it. You don't have to retrieve the source code in ST.com anymore.
It is compatible with STEdgeAI 2.1 for the deployment.