Skip to main content
CShen.1
Visitor II
September 22, 2021
Question

Deploy NN models on STM32L4R5ZI-P

I'm new to use STM32 boards. I have encountered problems when I try to deploy a pre-trained NN model on STM32L4R5ZI-P. When I have converted my NN model by using STM32cubeAI embedded in STM32cubeMX. It gives me a project folder. What should I use to flash the project to the board? Only IAR Embedded IDE?

  • Do I have another option like using STM32cubeIDE?
  • And how can I do that?
  • And how can I monitor the output from the board?

PS: I'm really confused about all these STM32 softwares, they are so many and barely know which one is doing what....

This topic has been closed for replies.

1 reply

Sara BEN HADJ YAHYA
ST Technical Moderator
October 29, 2021

Hi @CShen.1​ ,

Could you please share your .ioc file and specify which STM32CubeMX version are you using.

Regards,

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.