Skip to main content
Associate II
April 3, 2024
Question

Debugging problem

Hello,

I generated the C-code for my AI model using Cube AI, and I'm struggling with how to correctly set up the function calls and everything to initialize & run my model on Cube IDE. I made these first lines to verify if the returns were working fine for the initialization part:

ai_handle myNetwork = NULL;
ai_network_params params;
ai_error err;

err = ai_network_create(&myNetwork, AI_NETWORK_DATA_CONFIG);
if (err.type == AI_ERROR_NONE) printf("Network instance created\r\n");
if (ai_network_data_params_get(&params)) printf("Valid configuration is present\r\n");
if(ai_network_init(myNetwork, &params)) printf("Network initialized\r\n");

When debugging, I could get the proper return for the ai_network_create and ai_network_data_params_get, but I wasn't being able to initialize the network. Going further, I saw inside ai_network_init declaration:

ai_bool ai_network_init(
ai_handle network, const ai_network_params* params)
{
ai_network* net_ctx = ai_platform_network_init(network, params);
if (!net_ctx) return false;

ai_bool ok = true;
ok &= network_configure_weights(net_ctx, params);
ok &= network_configure_activations(net_ctx, params);

ok &= ai_platform_network_post_init(network);

return ok;
}

And in my case, the problem happens on the line "ok &= network_configure_activations(net_ctx, params)", where ok goes back to false. Going inside this function as well, I found the origin of the problem:

"if (ai_platform_get_activations_map(g_network_activations_map, 1, params)) {"

This condition is false. In order to work properly, it should be true. This is declared in the function "ai_platform_interface.h" as follows:

ai_bool ai_platform_get_activations_map(
ai_ptr* map, const ai_size map_size, const ai_network_params* params);

 

I don't know exactly how to proceed to solve this issue, and in general I'm struggling to set up the functions to run my model. Could someone help me please? Thanks!

 

This topic has been closed for replies.

1 reply

Visitor II
July 13, 2024
Hello, I also encountered the same problem, may I ask you to solve it