Skip to main content
Associate II
Nov 17, 2025 4:11 PM UTC
Question

Custom model object detection on STM32N6-DK error

Hi,

I have build a custom model based on st yolox model.
This model have an input of 480x480. Intput int8 and output float.
Five classes for vehicles detection
Quantized and tested on stm32N6570-DK.
Now i'm trying to add my model on this st example
https://github.com/STMicroelectronics/STM32N6-GettingStarted-ObjectDetection/tree/main
I'm following this tutorial to deploy my model
https://github.com/STMicroelectronics/STM32N6-GettingStarted-ObjectDetection/blob/main/README.md#application-build-and-run---dev-mode

I'm using stm32cubdeIDE to program the card
After i programmed the network_data.hex, i'm trying to deploy and debug the application.
But i have this error at this step : app_postprocess_init
The parameters

2025-11-17_16h12_42.png

2025-11-17_17h08_34.png

 

Do you have en idea how i can resolve this ?

11 replies

Julian E.
ST Technical Moderator
Nov 19, 2025 12:56 PM UTC

Hi @mls,

Did you edit the app_config.h and the post processing for your model needs?

Please look at this document:

STM32N6-GettingStarted-ObjectDetection/Doc/Deploy-your-tflite-Model-STM32N6570-DK.md at main · STMicroelectronics/STM32N6-GettingStarted-ObjectDetection

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
mlsAuthor
Associate II
Nov 19, 2025 2:07 PM UTC

Hi @Julian E.

I found the solution for my first issue ! I quantized a model in int8 (input) and float (output)....not supported in your example.
I quantized my model in uint8/int8 

#define POSTPROCESS_OD_ST_YOLOX_UI (106) /* ST YoloX postprocessing; Input model: uint8; output: int8 */


Downloaded the model in the card and launch the debug
Now stuck in Run Inference

mls_0-1763561213766.png

 

A question ? does the model need to be quantized in input in UINT8 or it could be INT8 ?


Julian E.
ST Technical Moderator
Nov 19, 2025 3:41 PM UTC

Hello @mls,

 

I think your issue is maybe due to a conflict between the input and output type your model use, you used in the generate command and what the firmware expect (as described in app_config.h)

 

Can you share the exact command you used (the generate) and your app_config.h

 

Also, if you can share your model, it would be helpful (in private message if you want).

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
mlsAuthor
Associate II
Nov 19, 2025 3:54 PM UTC

Hi @Julian E. 

Unfortunately for the moment i don't have access to my GPU server (thank you OVH ...) that i used to train the model.
That i did today is to quantize my model (h5 file) with ST Edge AI Developer Cloud.

mls_1-1763567476705.png

All the process is ok 

 

mls_2-1763567546276.png

See here the app_config.h

I will send you the model by private message

 

 

 

 

 

mlsAuthor
Associate II
Nov 26, 2025 5:18 PM UTC

Hi @Julian E. ,

Yes there are probably some inference but nothing that is displaying on the lcd screen.
Let me know if you make some progress on that. We are also testing Alif solution to make a choose on our futur platform to replace our nvivia solutions ...

Regards,

Mickaël

mlsAuthor
Associate II
Nov 28, 2025 11:14 AM UTC

Hi @Julian E. ,

Did you make some progress ?

This morning, tried with st_yolo_x_nano_480_1.0_0.25_3_st_int8.tflite original model. Same issue ...

Julian E.
ST Technical Moderator
Dec 12, 2025 10:29 AM UTC

Hi @mls,

 

manual deployment:

  • copy your model: STM32N6-GettingStarted-ObjectDetection\Model
  • Run the following commands
stedgeai generate --model your_model --target stm32n6 --st-neural-art default@user_neuralart_STM32N6570-DK.json --input-data-type uint8 --output-data-type int8
cp st_ai_output/network.c STM32N6570-DK/
cp st_ai_output/network_ecblobs.h STM32N6570-DK/
cp st_ai_output/network_atonbuf.xSPI2.raw STM32N6570-DK/network_data.xSPI2.bin
arm-none-eabi-objcopy -I binary STM32N6570-DK/network_data.xSPI2.bin --change-addresses 0x70380000 -O ihex STM32N6570-DK/network_data.hex
  • use STM32CubeProgrammer to flash the weights in STM32N6-GettingStarted-ObjectDetection\Model\STM32N6570-DK\network_data.hex
  • Edit STM32N6-GettingStarted-ObjectDetection\Application\STM32N6570-DK\Inc\app_config.h

In your case, you have 5 classes and are using a yolox with input shape 480x480:

/**
******************************************************************************
* @file app_config.h
* @author GPM Application Team
*
******************************************************************************
* @attention
*
* Copyright (c) 2023 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/

/* --------------- Generated code ----------------- */
#ifndef APP_CONFIG
#define APP_CONFIG

#include "arm_math.h"

#define USE_DCACHE

/*Defines: CMW_MIRRORFLIP_NONE; CMW_MIRRORFLIP_FLIP; CMW_MIRRORFLIP_MIRROR; CMW_MIRRORFLIP_FLIP_MIRROR;*/
#define CAMERA_FLIP CMW_MIRRORFLIP_NONE

#define ASPECT_RATIO_CROP (1) /* Crop both pipes to nn input aspect ratio; Original aspect ratio kept */
#define ASPECT_RATIO_FIT (2) /* Resize both pipe to NN input aspect ratio; Original aspect ratio not kept */
#define ASPECT_RATIO_FULLSCREEN (3) /* Resize camera image to NN input size and display a fullscreen image */
#define ASPECT_RATIO_MODE ASPECT_RATIO_FIT

/* Postprocessing type configuration */
#define POSTPROCESS_TYPE POSTPROCESS_OD_ST_YOLOX_UI

#define NN_HEIGHT (480)
#define NN_WIDTH (480)
#define NN_BPP 3

#define COLOR_BGR (0)
#define COLOR_RGB (1)
#define COLOR_MODE COLOR_RGB
/* Classes */
#define NB_CLASSES (5)
#define CLASSES_TABLE const char* classes_table[NB_CLASSES] = {\
 "bicycle" , "motorcycle" , "car" , "bus" , "truck"}\

/* Postprocessing ST_YOLO_X configuration */
#define AI_OD_ST_YOLOX_PP_NB_CLASSES (5)
#define AI_OD_ST_YOLOX_PP_L_GRID_WIDTH (60)
#define AI_OD_ST_YOLOX_PP_L_GRID_HEIGHT (60)
#define AI_OD_ST_YOLOX_PP_L_NB_INPUT_BOXES (AI_OD_ST_YOLOX_PP_L_GRID_WIDTH * AI_OD_ST_YOLOX_PP_L_GRID_HEIGHT)
#define AI_OD_ST_YOLOX_PP_M_GRID_WIDTH (30)
#define AI_OD_ST_YOLOX_PP_M_GRID_HEIGHT (30)
#define AI_OD_ST_YOLOX_PP_M_NB_INPUT_BOXES (AI_OD_ST_YOLOX_PP_M_GRID_WIDTH * AI_OD_ST_YOLOX_PP_M_GRID_HEIGHT)
#define AI_OD_ST_YOLOX_PP_S_GRID_WIDTH (15)
#define AI_OD_ST_YOLOX_PP_S_GRID_HEIGHT (15)
#define AI_OD_ST_YOLOX_PP_S_NB_INPUT_BOXES (AI_OD_ST_YOLOX_PP_S_GRID_WIDTH * AI_OD_ST_YOLOX_PP_S_GRID_HEIGHT)
#define AI_OD_ST_YOLOX_PP_NB_ANCHORS (3)
static const float32_t AI_OD_ST_YOLOX_PP_L_ANCHORS[2*AI_OD_ST_YOLOX_PP_NB_ANCHORS] ={30.000000, 30.000000, 4.200000, 15.000000, 13.800000, 41.999999};
static const float32_t AI_OD_ST_YOLOX_PP_M_ANCHORS[2*AI_OD_ST_YOLOX_PP_NB_ANCHORS] ={15.000000, 15.000000, 2.100000, 7.500000, 6.900000, 21.000000};
static const float32_t AI_OD_ST_YOLOX_PP_S_ANCHORS[2*AI_OD_ST_YOLOX_PP_NB_ANCHORS] ={7.500000, 7.500000, 1.050000, 3.750000, 3.450000, 10.500000};
#define AI_OD_ST_YOLOX_PP_IOU_THRESHOLD (0.5)
#define AI_OD_ST_YOLOX_PP_CONF_THRESHOLD (0.6)
#define AI_OD_ST_YOLOX_PP_MAX_BOXES_LIMIT (100)
#define WELCOME_MSG_1 "best_model_PerChannel_quant_int8_float32_random_1.tflite"
#define WELCOME_MSG_2 "Model Running in STM32 MCU internal memory"

#endif /* APP_CONFIG */

 Finally, open the cubeIDE project to build and run it

 

With Model zoo:

  1. copy your model in \stm32ai-modelzoo-services\object_detection\models
  2. edit user_config.yaml
general:
 model_path: ./models/best_model_PerChannel_quant_int8_float32_random_1.tflite
 model_type: st_yolo_x
operation_mode: deployment

dataset:
 class_names: [bicycle, motorcycle, car, bus, truck]

preprocessing:
 rescaling:
 scale: 1/255
 offset: 0
 resizing:
 aspect_ratio: fit
 interpolation: nearest
 color_mode: rgb

data_augmentation:
 random_contrast:
 factor: 0.4
 random_brightness:
 factor: 0.3
 random_flip:
 mode: horizontal
 random_translation:
 width_factor: 0.15
 height_factor: 0.15
 fill_mode: reflect
 interpolation: nearest
 random_rotation:
 factor: 0.02
 fill_mode: reflect
 interpolation: nearest
 random_crop:
 crop_center_x: (0.25, 0.75)
 crop_center_y: (0.25, 0.75)
 crop_width: (0.6, 0.9)
 crop_height: (0.6, 0.9)
 change_rate: 0.9

training:
 model:
 input_shape: (480, 480, 3)
 depth_mul: 1.0
 width_mul: 0.25
 dropout: null
 batch_size: 64
 epochs: 550
 optimizer:
 Adam:
 learning_rate: 0.0025
 callbacks:
 LRWarmupCosineDecay:
 initial_lr: 1.0e-05
 warmup_steps: 20
 max_lr: 0.00125
 hold_steps: 20
 decay_steps: 500
 end_lr: 1.0e-06
 EarlyStopping:
 monitor: val_loss
 patience: 60
 restore_best_weights: true
 verbose: 1

postprocessing:
 yolo_anchors: [0.5, 0.5, 0.07, 0.25, 0.23, 0.7]
 confidence_thresh: 0.4
 NMS_thresh: 0.5
 IoU_eval_thresh: 0.5
 plot_metrics: false
 max_detection_boxes: 20

quantization:
 quantizer: TFlite_converter
 quantization_type: PTQ
 quantization_input_type: uint8
 quantization_output_type: float
 export_dir: quantized_models
 
tools:
 stedgeai:
 version: 10.2.0
 optimization: balanced
 on_cloud: False
 path_to_stedgeai: C:/ST/STEdgeAI/2.2/Utilities/windows/stedgeai.exe
 path_to_cubeIDE: C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/stm32cubeide.exe

deployment:
 c_project_path: ../application_code/object_detection/STM32N6/
 IDE: GCC
 verbosity: 1
 hardware_setup:
 serie: STM32N6
 board: STM32N6570-DK

mlflow:
 uri: ./src/experiments_outputs/mlruns

hydra:
 run:
 dir: ./src/experiments_outputs/${now:%Y_%m_%d_%H_%M_%S}
 
  • run: python stm32ai_main.py

 

please note that you can have any input and output type for your model. When generating the C model, the model is edited to have uint8 input and int8 output:

stedgeai generate --model st_yolo_x_nano_480_1.0_0.25_3_st_int8.tflite --target stm32n6 --st-neural-art default@user_neuralart_STM32N6570-DK.json --input-data-type uint8 --output-data-type int8
 
Then you need to use the  POSTPROCESS_OD_ST_YOLOX_UI postprocessing
 
In the model zoo yaml, you should take a look at the postprocessing, mainly the number of boxes and the threshold. 
 
Have a good day,
Julian
​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
mlsAuthor
Associate II
Dec 12, 2025 2:04 PM UTC

Hi Julian,

Thank you  for your answer. Just tested your flow but same result. Whit my model it didn't work ..

mls_0-1765548258134.png

Have you tested with my model ??

Julian E.
ST Technical Moderator
Dec 12, 2025 2:36 PM UTC

@mls, yes I think, except if I did a mistake...
Your model are best_model_PerChannel_quant_int8_float32_random_1 and best_model_PerChannel_quant_int8_int8_random_1 correct?

 

Could you try to clone the repository again to make sure we are aligned?

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate III
Jul 10, 2026 3:17 PM UTC

hey was your issue resolved if yes how