fauvarque.danielBest answer
ST Employee
Jul 16, 2019 10:24 AM UTC
In your project you deactivated X-Cube-AI 3.4.0 and activated X-Cube-AI 4.0.0 but both are present. This causes problem in the generated code where you have both generated.
As we don't support yet migration of projects from a previous version to the current one, I recommend starting a new project a generating the code.
Last point you have generated the code using the Advanced structure option. The AI plugin still generates the file under Src and not under Core/Src.
It seems that using the option the order of the c files in the linker command is not correct. In order to be able to link correctly you have to move the files under Src into the Core/Src directory.
This last bug will be fixed in the next release.
Regards
Daniel
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.