Skip to main content
JNord
Associate II
April 1, 2019
Question

Commandline tool for converting models with X-CUBE-AI

Hi,

I made a small Python script that allows to convert models from the commandline. Wraps the same tools used by STM32CubeMX but can be integrated into build scripts and similar, without having to go through the GUI.

It also outputs the resources used (RAM,FLASH,CPU) . There are options for the compression settings, see `--help` for details.

Tested with Keras on Linux, but should work on other platforms too.

Example usage:

$ XCUBEAI_VERSION=3.4.0 python3 stm32convert.py mobilenet.hdf5 ./out/
 
Wrote model to ./out/
Model status: {"maccs_frame": 1639034, "flash_usage": 31150.0, "ram_usage_max": 216820.0, "ram_usage_min": 216820.0}
 
$ ls -a out/
. .. config.ai network.c network_data.c network_data.h network.h network.hdf5 network.json network.png

Hope this can be useful to others as well.

Regards, Jon Nordby

Machine Learning Engineer & Consultant

    This topic has been closed for replies.