Skip to main content
Evelina CAMILLERI
ST Employee
Jul 8, 2020 2:00 AM UTC
Solved

Can we program MLC without ST apps or without ST development boards?

 [webinar - Program decision trees in sensors with a Machine Learning Core]

This topic has been closed for replies.
Evelina CAMILLERI
ST Employee
Jul 8, 2020 2:03 AM UTC

The Machine Learning Core (MLC) configuration has to be created with the Unico GUI, since it contains all the specific hardware settings of the ST devices. Unico GUI can also run offline, in order to create a configuration even without any ST development board connected to the PC. 

Once the device configuration has been created with Unico (.ucf or .h file), it can be flashed on ST sensors featuring the MLC capability as shown by the example available on the ST GitHub repository. 

1 reply

Evelina CAMILLERI
Evelina CAMILLERIAuthorBest answer
ST Employee
Jul 8, 2020 2:03 AM UTC

The Machine Learning Core (MLC) configuration has to be created with the Unico GUI, since it contains all the specific hardware settings of the ST devices. Unico GUI can also run offline, in order to create a configuration even without any ST development board connected to the PC. 

Once the device configuration has been created with Unico (.ucf or .h file), it can be flashed on ST sensors featuring the MLC capability as shown by the example available on the ST GitHub repository.