Hi @Amith_lal ,
Yes, you can use another MCU and you can also not use Unicleo but use the .h file which is a C header file that can be included in any firmware, you have to scroll through the array contained in the header file and perform the operations described.
You can refer to the example on github, in particular to this snippet:
// load device configuration
for (uint32_t i = 0; i < sizeof(ispu_conf) / sizeof(ucf_line_ext_t); i++) {
if (ispu_conf[i].op == MEMS_UCF_OP_WRITE)
write(ispu_conf[i].address, ispu_conf[i].data); // write to device
else if (ispu_conf[i].op == MEMS_UCF_OP_DELAY)
delay(ispu_conf[i].data); // delay in ms
}
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.