Skip to main content
Paddykool
Associate
August 21, 2022
Solved

Can STM32WL be used with STM32Cube.AI ?

Noob question - can I use AI with the STM32WL SoC ?

I want to train a model and then use STM32Cube.AI to put it on STM32WLE5CC. This is so I can use AI on the end device and transmit data using LoRa all using the one chip.

Is this possible ?

Many thanks in advance.

This topic has been closed for replies.
fauvarque.daniel
fauvarque.danielBest answer
ST Employee
August 22, 2022

Yes STM32Cube.AI is supported on the STM32WL MCUs

Regards

Daniel

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

2 replies

fauvarque.daniel
fauvarque.danielBest answer
ST Employee
August 22, 2022

Yes STM32Cube.AI is supported on the STM32WL MCUs

Regards

Daniel

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Paddykool
PaddykoolAuthor
Associate
August 24, 2022

Awesome thank you!