Question
Can NanoEdge AI be used for non-classifications?
I need to tune PID coefficients for a set of motor controllers. I’d like to use NanoEdge AI studio, but I’m not sure it supports what I need. The input to the model is to be a set of four error values and the output is a set of coefficients. NanoEdge accepts UART input for the error values, which is perfect, but I need it to generate coefficients. Instead, I only see examples of it being used for classification tasks. Can it be used for this? If not, is there another tool?