Skip to main content
Associate III
Nov 9, 2026 2:19 PM UTC
Question

build error when re-generating code pf a cubeAIstudio project using cubeMX

Hello there,
I have encountered an issue using cubeAIstudio
I first had it with the V1.2  and still having it even when using the new 1.4 version
everything works fine when I make a run  and generate the hole project (built with 0 errors)
but when I open the .ioc file project using cubeMX and add some other features like(exampel : uart) and re-generate the code)
I get this error

 I understand that its a middleware related issue
so I tried to save the original AI middleware folder and paste it again after re-generating the code after adding any other peripehral
but same issue
So is there a quick fix to this or will it be fixed in newer versions.
os I’am just doing something wrong?