Skip to main content
Associate
Jul 26, 2024 12:33 PM UTC
Question

Assistance with TensorFlow-Lite Model Porting on NUCLEO-F401RE Board

Hi,

I'm encountering an issue while porting a trained TensorFlow-Lite model, obtained from a research paper, onto a NUCLEO-F401RE board. The process goes smoothly when analyzing and validating the code on my desktop, generating the code, and downloading it to the board. However, when I attempt to perform a "validate of target," I receive an "Invalid firmware" error (screenshot attached). The model is neural network based on U-Net architecture with shallow structure, single-channel input, and output.

Board used: NUCLEO-F401RE

STM32MX : Version 6.12.0

STM32CubeIDE : Version: 1.16.0

Could you please provide guidance on how to resolve this issue? Any suggestions for modifications or troubleshooting steps would be greatly appreciated.

Thank you!

This topic has been closed for replies.

1 reply

fauvarque.daniel
ST Employee
Aug 28, 2024 8:43 AM UTC

Please verify in the log that the firmware has been correctly compiled and flashed on the target

You can retreive the logs in ~/.stm32cubemx/STM32CubeMX.log

Regards

Daniel

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.