Skip to main content
Yjang.1
Associate II
March 24, 2021
Question

Are there any easier examples or tutorials for loading the pre-trained model to external memory?

Hello, I have a STM32F746G-DISCO which has a microcontroller with 1 Mbytes of Flash memory and 340 Kbytes of RAM. However, I would need more space for my bigger Keras models.

I have seen examples of code in the new function pack FP-AI-VISION1 which is providing a Computer Vision AI example of food classification. It is also providing different memory configurations : use of internal Flash vs external Flash, internal RAM vs external SDRAM.

​

However, since i am a beginner, it's difficult to write code from scratch and access and use external memory, and all these processes are not well understood.​

Are there any easier examples or tutorials for loading the pre-trained model to external memory? 

Best regards,

This topic has been closed for replies.