Skip to main content
martinj3456
Associate III
August 15, 2019
Question

Any DCMI based Image classification example?

  • August 15, 2019
  • 3 replies
  • 1582 views

Hello everyone,

It's good to see a number of tutorials/implementations posted by community members which encourage beginners like me to implement AI at the microcontroller level.

Is there any complete image classification example or tutorial where ST microcontroller capture images via DCMI interface and immediately classify images using the pre-trained network?

If available, I sincerely request to share the link.

Thanks in advance,

M

This topic has been closed for replies.

3 replies

Matthieu
ST Employee
August 16, 2019

Hello,

The new function pack FP-AI-VISION1 is providing what you are looking for: a Computer Vision AI example of food classification from DCMI camera.

The function pack is based on STM32H747 Discovery board and you can find it here:

https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/fp-ai-vision1.html

Best Regards,

Matthieu

martinj3456
Associate III
August 16, 2019

Hello Matthieu,

Thank you for your reply. yes, this is a great starting point.

Is the Keras CNN model employed in these application open source? I mean, I'll use custom images to re-train the model.

May be your model (github project) would be helpful to follow the steps and implement a new model for the custom image set.

Thank you.

Matthieu
ST Employee
August 17, 2019

​Hello,

A Keras CNN model is provided (under ST free license) as part of the package as well as the quantization scripts so you can retrain and quantize on your own image dataset?

Best Regards

Matthieu