Skip to main content
M.Mardini
Associate II
July 12, 2023
Solved

Anomaly detection argumente,

Hello every Body, i am investigating the use of ISM330IS with nanoEdgeAI to detect Anomaly situations.

 

Lets take a motor for air conditioning as an example, If the motro  has protection against high current, and a tachometer, What are the benefits of ISPU  against those typical protection.

the seconde question is ,is there any industrial project using the ISPU to detect anomality ?

 

thank you very much

This topic has been closed for replies.
niccolò
niccolòBest answer
ST Employee
July 13, 2023

Hi @M.Mardini ,

when you use ISPU to detect anomalies, you are searching for differences in the movements between the normal functioning of the device and a faulty one. This means that you can also manage to detect a problem that the other two methods are not able to detect, like a strange movement on one of the axis.
at the moment, there are no industrial project available, but I think there are people already working on it =)

Niccolò

1 reply

niccolò
niccolòBest answer
ST Employee
July 13, 2023

Hi @M.Mardini ,

when you use ISPU to detect anomalies, you are searching for differences in the movements between the normal functioning of the device and a faulty one. This means that you can also manage to detect a problem that the other two methods are not able to detect, like a strange movement on one of the axis.
at the moment, there are no industrial project available, but I think there are people already working on it =)

Niccolò