Skip to main content
Umahe.1
Associate II
May 18, 2022
Question

Analyze is failing and got error as NOT IMPLEMENTED: Transpose of batch not supported Got the above error while analyzing the tfltie model in STMCubeMX

  • May 18, 2022
  • 4 replies
  • 1178 views

I have an AI model that detects the human activity and saved the model in .h5 format and converted it into .tflite image. When I upload the image into STMCubeMX and analyze the model, analyze is failing and showing as NOT IMPLEMENTED: Transpose of batch not supported.

Need help with the resolution for above issue. Thanks in Advance.

    This topic has been closed for replies.

    4 replies

    fauvarque.daniel
    ST Employee
    May 18, 2022

    Does the Keras model pass in X-CUBE-AI ?

    Could you share the tflite model so we could have a look

    ​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
    Umahe.1
    Umahe.1Author
    Associate II
    May 18, 2022

    Thanks for the response and have attached the model.

    fauvarque.daniel
    ST Employee
    May 18, 2022

    I can reproduce your error with your model, thanks.

    I see that your network is in float, did you try to directly import the h5 Keras model ? as X-Cube-AI natively supports Keras it is better to take the original model rather than a transformed one

    Regards

    ​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
    Umahe.1
    Umahe.1Author
    Associate II
    May 19, 2022

    I'm Okay if my model predicts and throws output in float, I just want the model to work with MCU.

    Tried with h5 model and seeing this error:

    INTERNAL ERROR: The layer has never been called and thus has no defined input shape.