Skip to main content
MSant.11
Associate III
September 5, 2021
Question

After analyzing a tflite network with X-CUBE-AI, I get the warning " NOT IMPLEMENTED: Shape with 1 dimensions not supported: (15600,)". How can I fix this issue ? Thank you

..

    This topic has been closed for replies.

    4 replies

    JTedot
    Associate III
    September 6, 2021

    Same problem, still no answer. Judging by your specific input, you want to use YAMNet on embedded devices as well, right?

    MSant.11
    MSant.11Author
    Associate III
    September 6, 2021

    Yes, I wish.

    Do you know working sound classifications, that can be used as well in embedded STM board ?

    JTedot
    Associate III
    September 6, 2021

    Self-trained models seem to work. Check out this article: https://www.kdnuggets.com/2020/02/audio-data-analysis-deep-learning-python-part-1.html

    At the end, you could convert your model via

    import tensorflow as tf
    converter = tf.lite.TFLiteConverter.from_keras_model(model)
    tflite_model = converter.convert()
    open("my_model.tflite", "wb").write(tflite_model)

    and pass that to the X Cube AI. It passes the analysis correctly. I'm thinking about dropping YAMNet on embedded systems, since too many functions happen abstractly under the hood and aren't really accessible. If you build your own model, you are in full control, but you also have to extract features yourself. You can't pass a network an audio file, you have to pass it a highly filtered spectrogram (in essence audio classification is image classification).

    MSant.11
    MSant.11Author
    Associate III
    September 6, 2021

    Thank you!

    Do you have any experience with FP-AI-SENSING1 and its Middleware ASC (acoustic scene classification) ?

    https://www.st.com/en/embedded-software/fp-ai-sensing1.html