Skip to main content
ACapo
Associate II
Apr 2, 2019 9:24 AM UTC
Solved

Activations may exeed the size of all SRAM segments

I am trying to deploy a pre-trained Mobilenet model using STMCubeMX.ai, but I am facing some issue that I want to report.

Here the link of the project

https://github.com/alessandrocapotondi/mobilenet_stmcube_ai

Here the model I am using:

https://github.com/alessandrocapotondi/mobilenet_stmcube_ai/blob/master/keras_model/mobilenet_160_0_25.h5

Here the resource usage of my model:

0690X0000089fpeQAA.png

600KB RAM for the activations and 1.79MB of weights. Unfortunally despite the "Green Light" given by the tool for the deployment on the STMH7432ZI on the device there is no segment that can fit such ammont of contigous data.

/* Specify the memory areas */
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
}

Best,

Alessandro

This topic has been closed for replies.
jean-michel.dBest answer
ST Employee
Apr 2, 2019 9:59 AM UTC

​Hello,

You have absolutly rights, unfortunaltly this check is currently not correctly supporting by the X-CUBE-AI tools.

br,

Jean-Michel

4 replies

jean-michel.dBest answer
ST Employee
Apr 2, 2019 9:59 AM UTC

​Hello,

You have absolutly rights, unfortunaltly this check is currently not correctly supporting by the X-CUBE-AI tools.

br,

Jean-Michel

ACapo
ACapoAuthor
Associate II
Apr 2, 2019 10:14 AM UTC

Really thanks for your support!

Bassett.David
Associate III
Apr 2, 2019 12:49 PM UTC

As an aside - I like your test image!!!

ACapo
ACapoAuthor
Associate II
Apr 2, 2019 1:10 PM UTC

:>