Skip to main content
Associate II
Aug 11, 2026 3:38 AM UTC
Question

ABI conflict between X-CUBE-AI runtime and STM32H7 Safety STL with ArmClang

I am integrating X-CUBE-AI and the STM32H7 Safety STL into the same STM32H743 Keil/ArmClang project.

The X-CUBE-AI Keil runtime requires short enums and 16-bit wchar_t (-fshort-enums -fshort-wchar). However, the Safety STL library appears to require full-size enums and 32-bit wchar_t.

Configuring the project for X-CUBE-AI causes the Safety STL library to fail linking. Configuring it for the Safety STL causes Arm linker ABI errors when linking the X-CUBE-AI runtime, including enum-size and wchar_t mismatches.

Is there an officially supported compiler configuration or compatible library variant that allows X-CUBE-AI and the STM32H7 Safety STL to coexist in the same ArmClang application?