Skip to main content
Oleksandr_Gonchar
Associate
May 18, 2023 11:32 AM UTC
Solved

Why I can't set HOST_DEBUG_EN in TnDCM CR register on SR6P7G7C7? I use key 0xE0E05FE0 to unlock it, but bit doesn't change the value. External debugger is not connected.

I'm working with SR6P7G7C7 and I would like to start CoreSight trace from MCU without external tools. I configured Core0 ETM and TMC ETR, but trace doesn't start. I assume the problem is in TnDCM_CR register, I am not able to set HOST_DEBUG_EN. I use the key like below:

#define TnDCM_CR (*(volatile uint32_t*)(0x7100c000))
 
TnDCM_CR = 0xE0E05FE0;
TnDCM_CR = 0x10000000;

but it doesn't change the value in register.

This topic has been closed for replies.
Salvatore Maria MESSINA
ST Employee
May 25, 2023 4:21 PM UTC

Hello,

If JCOMP is floating and debugger is not connected, this bit is used to enable host based debugging. By default when debugger is not connected (and JCOMP is floating or connected to GND), debug and trace logic remains in reset. Setting this bit to HIGH will bring the debug and trace resources out-of-reset. When any CPU or non-CPU Bus Master needs to access the debug and trace

resources it should first program this bit to HIGH. HOST_DEBUG_EN

overwrites the JCOMP or TAP select signal connected to DAP reset.

0 When debugger is not connected then host based debugging is not

enabled. JCOMP to DAP is low.

1 When debugger is not connected then host based debugging is

enabled. JCOMP to DAP is high.

So, if you connect the hardware debugger tool means that JCOMP is configured to enable device debug part, so it will work independently by this bit configuration.

Regards,

Salvo

10 replies

Salvatore Maria MESSINA
ST Employee
May 23, 2023 10:01 AM UTC

What is the JCOMP configuration of the DAP connector? As the debugger is not connected, is it floating? Or do you force this pin to 1. If you don't use any hardware configuration, can you try to set a logic value 1 on JCOMP pin?

Oleksandr_Gonchar
Associate
May 23, 2023 2:37 PM UTC

JCOMP pushed up

Oleksandr_Gonchar
Associate
May 23, 2023 11:02 AM UTC

JCOMP pushed up


_legacyfs_online_stmicro_images_0693W00000bkfEiQAI.png

Salvatore Maria MESSINA
ST Employee
May 23, 2023 2:47 PM UTC

Are you able to read the TnDCM SR?

What is the flow that you followed before accessing CR?

Oleksandr_Gonchar
Associate
May 24, 2023 2:35 PM UTC

Yes, I am able to read it out and result looks strange for me.

TnDCM SR has always the same value 0x311303 despite debugger connected or not connected. I read it by MCU and send the value over UART.

About flow, I tried set it in startup code before the Exception level is switched in System Mode and before MPU initialisation, but it didn't help. So I put the code direct after vector table setup, the code is below:

 ldr r0, =#0x7100c000
 ldr r1, =#0xE0E05FE0
 str r1, [r0]
 ldr r1, =#0x10000000
 str r1, [r0]

But it didn't help in general.

I assume it worked only once, but after that I lost a control over my board, the debugger now doesn't see JTAG connection with my Stellar, it looks like now it is bricked. I guess it was bad idea put this code in startup. But before the board was bricked, I ran this code many times without any effect. For the moment I have a new board, but this code doesn't work also.

Salvatore Maria MESSINA
ST Employee
May 25, 2023 5:49 AM UTC
Hello,

It could be to MPU configuration. I suggest to put code in EL2 after MPU configuration for.

I don't think the code can brick the device.


ST Restricted
May 23, 2023 5:39 PM UTC

Hi Oleksandr,

Thank you for contacting STMicroelectronics. Your inquiry is being treated directly via the online support team.

Should anyone have similar technical inquiries regarding an ST device, please do not hesitate to submit your requests directly at my.st.com/ols.

Kind Regards,

Christian

ST Support

Salvatore Maria MESSINA
ST Employee
May 25, 2023 4:21 PM UTC

Hello,

If JCOMP is floating and debugger is not connected, this bit is used to enable host based debugging. By default when debugger is not connected (and JCOMP is floating or connected to GND), debug and trace logic remains in reset. Setting this bit to HIGH will bring the debug and trace resources out-of-reset. When any CPU or non-CPU Bus Master needs to access the debug and trace

resources it should first program this bit to HIGH. HOST_DEBUG_EN

overwrites the JCOMP or TAP select signal connected to DAP reset.

0 When debugger is not connected then host based debugging is not

enabled. JCOMP to DAP is low.

1 When debugger is not connected then host based debugging is

enabled. JCOMP to DAP is high.

So, if you connect the hardware debugger tool means that JCOMP is configured to enable device debug part, so it will work independently by this bit configuration.

Regards,

Salvo

Oleksandr_Gonchar
Associate
May 26, 2023 4:17 PM UTC

Ok, I got it.

Then maybe you can help me to understand, why the trace is not recorded in RAM region, where I expect to see it?

With External Debugger the Trace is working and I see it in RAM, but without I don't see it, the value is always 0x0.

Here is current TMC ETR and ETM configuration, which I se with my application on Core0;

 ETR_AXICTL

  ADDRESS:0x7c109110

  DATA:0xf00

 ETR_DBALO

  ADDRESS:0x7c109118

  DATA:0x64022000

 ETR_RSZ

  ADDRESS:0x7c109004

  DATA:0x2000

 ETR_CTL

  ADDRESS:0x7c109020

  DATA:0x1

 ETM_TRCPRGCTLR

  ADDRESS:0x7ec40004

  DATA:0x1

 ETM_TRCCONFIGR

  ADDRESS:0x7ec40010

  DATA:0x31fc7

 ETM_TRCSTALLCTLR

  ADDRESS:0x7ec4002c

  DATA:0x0

 ETM_TRCSTATR

  ADDRESS:0x7ec4000c

  DATA:0x0

 ETM_TRCOSLSR

  ADDRESS:0x7ec40304

  DATA:0x8

 ETM_TRCLSR

  ADDRESS:0x7ec40fb4

  DATA:0x1

 ETM_TRCPDSR

  ADDRESS:0x7ec40314

  DATA:0x1

 TnDCM_SR

  ADDRESS:0x7100c008

  DATA:0x311303