Skip to main content
Yannek
Associate III
Feb 7, 2020 9:22 AM UTC
Solved

Which FlexCAN modules are available in 3-CAN SPC582B?

Although SPC582B family has up to 7 FlexCAN modules, some units have only 3 (i.e. SPC582B60E1CD00X).

Which 3 of 7 CAN modules are available in this processor?

Since SPC5Studio shows 7 CANbuses for this processor, I don't know which I/O should I design for CANbuses.

This topic has been closed for replies.
Giuseppe DI-GIORE
ST Employee
May 8, 2020 10:52 AM UTC

This information will be published in DS rev4

6 replies

Erwan YVIN
ST Technical Moderator
Feb 7, 2020 2:21 PM UTC

Yes , in SPC5Studio , we are seeing 7 Can Buses

You can use the Pinmap Wizard in order to determine which I/O Buses are designed for CAN Bus

It is very useful.

I am checking in the RM.

and check with experts

Best regards

Erwan

0690X00000D8TrHQAV.png

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Yannek
YannekAuthor
Associate III
Feb 7, 2020 4:27 PM UTC

Unfortunately, in this case, I cannot use SPC5Studio to see which I/O pins are designed for CANbus in SPC582B60E1CD00X.

SPC5Studio shows that this processor has 7 CANbuses, while actually it has only 3.

In SPC5Studio there is no choice between SPC582B60E1CD00X (3 CANbuses) and SPC582B60E1MH00Y (7 CANbuses):

0690X00000D8UnfQAF.png

Waiting for the answer from experts :)

Yannek

JoniS
Senior
Feb 7, 2020 5:00 PM UTC

I bet you get the information faster from datasheet of the given mcu.​

Yannek
YannekAuthor
Associate III
Feb 7, 2020 5:20 PM UTC

I bet you don't, JoniS. Not only faster. Not at all.

Yannek
YannekAuthor
Associate III
Feb 12, 2020 3:32 PM UTC

Hi Erwan,

Would you have any information in this topic, please?

Our project stucked, because we don't know which pins should be used...

Best,

Yannek

Giuseppe DI-GIORE
ST Employee
May 8, 2020 10:52 AM UTC

This information will be published in DS rev4