Question
what is the difference between loopback mode and normal mode in CAN of SPC58NN84x (Bernina)
I am a thesis student and part of my thesis is to test the CAN of SPC58NN84x MCU in two modes, the normal mode, and the loopback mode.
The loopback mode is ok as the CAN receives the same message that it transmits properly, however, this is not the case in the normal mode as the transmission is always in "pending" and not successfully placed on the bus
The CAN controller is connected to a TJA1041 high speed can transceiver.
Can anybody tell me what is the difference between the two modes or a hint how could this be fixed and make the can works in the loopback mode properly?