Skip to main content
ZBen .11
Visitor II
Nov 13, 2020 10:34 AM UTC
Solved

What are the SW & HW tools to acess CAN bootloader on SPC5 eval boards

Hello community,

An automotive client that i'm working with wants to devolope his own bootloader basing on ST bootloader on SPC5 product. my mission is to validate this bootloader on SPC5 eval bord of ST.So , im asking if there is a specific HW and SW tools to validate CAN UDS bootloder. Also any documentation about CAN bootloader could help

Thinks in advance

Farmer ST engineer

Zied ben Amira

    This topic has been closed for replies.
    Giuseppe DI-GIORE
    ST Employee
    Nov 19, 2020 3:26 PM UTC

    Hello,

    open the microcontroller Reference Manual and look for Boot Assist Flash (BAF) chapter,

    read the section M_CAN download protocol.

    Regards,

    Giuseppe

    2 replies

    Giuseppe DI-GIORE
    ST Employee
    Nov 19, 2020 3:26 PM UTC

    Hello,

    open the microcontroller Reference Manual and look for Boot Assist Flash (BAF) chapter,

    read the section M_CAN download protocol.

    Regards,

    Giuseppe

    Associate III
    Feb 28, 2024 4:35 PM UTC

    Thanks Giuseppe,

    I was hoping there were something already done by ST ....

    But ... can I configure CAN as bootloader (SPC570Sxx Firmware Updater Component) and then 

    I will have to create only an host application to download the firmware via CAN?

    Fabio