Skip to main content
stefanodimascio9
Associate III
Nov 27, 2015 10:13 AM UTC
Question

using UART

Posted on November 27, 2015 at 11:13

Hello everybody,

I'm using the SPC56EL70L5DISP board.

In order to use UART, I put the jumpers in J18 and J20 to connect UART-MCU LIN0, following the board user guide.

Running the test example with UART and blinking LEDs, I try to read the hello world from a PC. I use a serial to USB adapter and a software configured for 38400-N-1 with no flow control or handshaking. I don't receive anything though.

I'm asking for a confirmation: should this work or did I miss something here?

Thanks in advance for the help.

#spc56 #uart
This topic has been closed for replies.

8 replies

Erwan YVIN
ST Technical Moderator
Nov 27, 2015 10:29 AM UTC
Posted on November 27, 2015 at 11:29

Hello Stefano ,

you have to take : SPC56ELxx OS-Less Test Application for DiscoveryPlus

yes , your jumper configuration is good.

JP18 and JP20 should be plugged on UART-MCU LIN0

38400 Bauds is the good default speed.

Anyway, i am checking the test application on SPC5Studio 3.7.1.

   Best Regards

                Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Erwan YVIN
ST Technical Moderator
Nov 27, 2015 2:33 PM UTC
Posted on November 27, 2015 at 15:33

Hello Stefano ,

the test application coming from SPC5Studio 3.7.1 ''SPC56ELxx OS-Less Test Application for DiscoveryPlus'' is working well

(Cf Screenshot)

you have to use the USB-COM Port driver from your USB Cable not the Virtual COM PORT (VCP) Generated by the FTDI Driver from SPC5-UDESTK

          Best regards

                         Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Erwan YVIN
ST Technical Moderator
Nov 27, 2015 2:38 PM UTC
Posted on November 27, 2015 at 15:38

Here is the screenshot

''my.st.com'' is lagging today

            Best regards

 

                     Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Erwan YVIN
ST Technical Moderator
Nov 27, 2015 2:45 PM UTC
Posted on November 27, 2015 at 15:45

I can not attach anymore a image file on my.st.com

...sorry for this issue ...

           Best regards

                            Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
stefanodimascio9
Associate III
Nov 27, 2015 4:38 PM UTC
Posted on November 27, 2015 at 17:38

I've only my cable COM in the device manager. VCP is not loaded in the FTDI driver and I can't connect any other COM. I've tried other PCs too and it doesn't work anyway. I'm going to check if D connector electrically works and to try with other cables.

Thank you, you're very helpful

Erwan YVIN
ST Technical Moderator
Nov 30, 2015 9:53 AM UTC
Posted on November 30, 2015 at 10:53

Hello Stefano ,

Could you check these jumper configurations ?

Best regards

Erwan

________________

Attachments :

DSC_0272.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0P0&d=%2Fa%2F0X0000000bYz%2F7mPVVBZFggcDB0uMEh5Om79JxNS2cCFe0sKENKsqDBs&asPdf=false
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
stefanodimascio9
Associate III
Nov 30, 2015 5:22 PM UTC
Posted on November 30, 2015 at 18:22

Thanks, this is my jumper configuration. I hope I will be able to try another cable and to check the DB9 connector soon. 

stefanodimascio9
Associate III
Dec 1, 2015 8:28 PM UTC
Posted on December 01, 2015 at 21:28

The problem was the chosen serial to usb adapter that doesn't work properly.Using another cable solved the problem. 

Thanks again!