Skip to main content
yjin.1
Associate II
Sep 23, 2021 12:31 AM UTC
Question

Using SPC584B MCU CAN FD and Standard CAN

I am planning to use SPC584B70 MCU.

During the review, I have a question in the datasheet.

​

​

In the custom version(6. Ordering information):

​

0 = 4x std CAN

D = 4x ISO CAN FD

G = 8x std CAN

H = 8x ISO CAN FD

E = 8x std CAN / Ethernet

M = 8x ISO CAN FD / Ethernet

​

​

If I choose D version, can't I use 'standard frame CAN'?

Can 'extended frame CAN' be used?

Likewise if I choose version 0, can I only use ISO CAN FD?

​

​

​

Please help me.

Thanks.

​

This topic has been closed for replies.

2 replies

Erwan YVIN
ST Technical Moderator
Sep 29, 2021 2:32 PM UTC

Hello yjin ,

SPC584B70 MCU is ISO CAN FD compliant.

it conforms with CAN protocol version 2.0 part A, B and ISO 11898-1: 2015

could you give your datasheet reference ?

According to the CAN FD.

  • CAN FD can be used Standard frame CAN network
  • 'extended frame CAN can not be used in an existing standard CAN network.
  • i am checking with experts for the last question.

Best Regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
yjin.1
yjin.1Author
Associate II
Sep 29, 2021 11:53 PM UTC

https://www.st.com/en/automotive-microcontrollers/spc584b70e3.html

​

In page 128, you will see following image :

0693W00000FAyuOQAT.jpg​

​

I need to select ordering information to order the spc584b70 mcu.

Among them, I am curious about the information about Custom Version (std CAN, ISO CAN FD, etc.).

CPU marked std CAN supports only standard/extended CAN (CAN 2.0A, 2.0B),

CPU marked ISO CAN FD supports standard/extended CAN(CAN 2.0A, 2.0B) + ISO CAN FD?

​or ISO CAN FD Only?

​

I am very much looking forward to your help.

Thank you!