Skip to main content
ssk
Associate III
Feb 18, 2015 11:25 AM UTC
Question

Using Data flash

Posted on February 18, 2015 at 12:25

Hello Members,

I am using SPC560D030 for my product. I want to use the Data flash to store the device configuration i.e. I want to use Data flash as NVM. The configuration data is of 120 bytes. I tried reading the reference manual (CD00259063.pdf) on using the Data flash as NVM but may be I am unable to understand on reading/writing to Data flash. I don't find any APIs for it. How can I use the 'DFLASH' for reading or writing? Any example code or document reference will be helpful.

Thanks in advance for any help.

Mike.

#dflash #dataflash #dataflash #orhan-y?lmaz #data-flash
    This topic has been closed for replies.

    16 replies

    orhanyilmaz
    Associate III
    Apr 29, 2015 2:23 PM UTC
    Posted on April 29, 2015 at 16:23 Hello Erwan, My test code

    #define DFLASH_BASE_ADDR 0x00800000
    ...
    Addr = DFLASH_BASE_ADDR;
    ..
    DFLASH.MCR.R = 0x00000010;
    (*(U_32 *)Addr) = data;
    DFLASH.MCR.R = 0x00000011;
    while(!(DFLASH.MCR.R & 0x00000400));
    DFLASH.MCR.R = 0x00000010;
    DFLASH.MCR.R = 0x00000000;

    but not work! Thanks
    Erwan YVIN
    ST Technical Moderator
    Apr 30, 2015 7:49 AM UTC
    Posted on April 30, 2015 at 09:49

    Hello Orhan ,

    I have tested the code this morning. Your code is working well , you have just to erase the block before writing a word. Did you initialize correctly the driver before ? (Cf Giovanni's code)

    /**
    * @brief Initializes the driver.
    */
    void
    spc5_dflash_init(
    void
    ) {
    /* Fixes wrong initialization in HAL driver.*/
    // CFLASH.PFCR1.R = 0x318D8081;
    CFLASH.PFCR1.B.BK1_APC = 3;
    CFLASH.PFCR1.B.BK1_RWSC = 6;
    /* Unlock procedure.*/
    DFLASH.LML.R = 0xA1A11111;
    DFLASH.LML.B.LME = 1;
    DFLASH.SLL.R = 0xC3C33333;
    DFLASH.SLL.B.SLE = 1;
    DFLASH.MCR.R = 0x0;
    /* All blocks unlocked.*/
    DFLASH.LML.B.LLK = 0;
    DFLASH.SLL.B.SLK = 0;
    }

    Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    orhanyilmaz
    Associate III
    Jun 1, 2015 2:52 PM UTC
    Posted on June 01, 2015 at 16:52

    Thanks Erwan. It's work!

    lizheng887
    Associate II
    Feb 26, 2016 5:49 AM UTC
    Posted on February 26, 2016 at 06:49

    Hi Erwan,

    I am using data flash on SPC560P40L1, and the eemprom emulation driver is used provided by spc5studio v3.7.

    There is something wrong when initialize, the return error code is 0x40(EE_ERROR_PE_OPT). However, the same code is running well on SPC560P50L5, and I need your help.

    I donot know where the problem is?

    Thanks.

      /* Init EEPROM.*/

      result = FSL_InitEeprom(&eepromConf, NULL_CALLBACK);

      if (result != EE_OK && result != EE_FIRST_TIME_INITIALIZATION) {

        //while (sd_lld_write(&SD1,(uint8_t*)''INIT ERROR\r\n'', 12) == SERIAL_MSG_WAIT);

        //return result;

      }

      /* Read dataID 0.*/

      result = FSL_ReadEeprom(&eepromConf, 0, (UINT32)(dtc_ram), NULL_CALLBACK);

    procolo
    Visitor II
    Feb 26, 2016 9:19 AM UTC
    Posted on February 26, 2016 at 10:19

    Hello,

    currently ee library only support SPC560P50 devices. We are introducing the support for SPC560P40/34 and this library will be available in the next version of SPC5Studio.

    Meanwhile, you can use the zip attached to solve the problem.In your project for P40 please replace the following files:

    - eed.a

    - eed_emulation,h

    Please not that

    • Every time you generate the project the eed.a files will be the old one , so you should replace again the library
    • this library only works for P if you want to use on P50 you should not use these files but the ones generated as usual.

    In the next version, the eed.a library will support both devices.

    Sorry for the inconvenience.

    Regards

    Procolo

    ________________

    Attachments :

    EEPROM.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Rs&d=%2Fa%2F0X0000000bZ4%2FdiL1XG101T81E3TbslvnKv2nAr1swzYyty2.vN3pQ9Y&asPdf=false
    lizheng887
    Associate II
    Apr 7, 2016 6:57 AM UTC
    Posted on April 07, 2016 at 08:57

    thanks.