Skip to main content
gilad2
Associate II
Apr 8, 2015 7:33 AM UTC
Question

unable to debug using SPC5-UDESTK

Posted on April 08, 2015 at 09:33

Hi there,

I am trying to run a test application (SPC560Bxx OS-Less test application) on SPC560B60L5 mounted in SPC560BADAPT144S evaluation board, using SPC5-UDESTK.

After generating and building the test application I am trying to connect by pressing hte debug button, but it says that launch failed, binary not found.

After creating a ''C/C++ Application'' debug configuration and pointing it at the out.elf file in the build directory, I am still failing to connect with the error:

Error while launching command: gdb --version.

Is there anything missing in my SPC5 installation?

Also, could someone point me at a step by step tutorial application notes? I was unable to find one in ST's site.

Thanks in advance.
    This topic has been closed for replies.

    3 replies

    Erwan YVIN
    ST Technical Moderator
    Apr 8, 2015 7:44 AM UTC
    Posted on April 08, 2015 at 09:44

    Hello Gilad ,

    You have to use the Debug Button from the activity wizard (SPC5Studio perspective).

    (Cf Screenshot)

    Do you install PLS-UDE Visual Platform for the debugging?

    Best Regards

    Erwan

    ________________

    Attachments :

    2015-04-08_094341.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWfs&d=%2Fa%2F0X0000000boT%2FrZ_LI1Ww9ZwWarLFKAUqHc0SBda3f6zbN7vPHaYi0MQ&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    gilad2
    gilad2Author
    Associate II
    Apr 8, 2015 12:56 PM UTC
    Posted on April 08, 2015 at 14:56

    Thanks Erwan, I was indeed missing the UDE installation.

    So now I am able to load and program the chip and even see the example application blinking a led, so that's great, but the CAN packets it is supposed to transmit are not showing.

    I can see in the pin wizard that surprisingly no pads are configured for any flexcan module, so I configured pb0 and pb1 to be flexcan0 pins (those are the pads physically connected to the high speed CAN transceiver on the evaluation board), but still no luck. 

    I regenerated the code after configuring the pin wizard, I assume that's what I was supposed to do?

    Also, for PB1, the RX CAN pad, I was unable to configure CAN0RX directly, but had to configure it as ''GPIO17 [WKPU4, CAN0RX]''.

    as a result I get the warning:

    Warning: PADSEL 'ps62' has not a valid selection. Pin 'PIN_GPIO17' set to 'NOT_USED'.

    and I am unable to find where to configure that ps62 so the signal will be routed to the flexcan0 module.

    I'd appreciate any help on the matter or also a referral to a document a begginer such as myself can read.

    Thanks.

    Erwan YVIN
    ST Technical Moderator
    Apr 10, 2015 8:30 AM UTC
    Posted on April 10, 2015 at 10:30

    Hello Gilad ,

    For PADSEL62, LIN0RX/LIN0TX is already set in this demo.(Cf Screenshot)

    (no need to set..)

    If you want to use CAN0TX/CAN0RX, you should disable LIN0RX/LIN0TX on others pins or used CAN1RX/CAN1TX.

    Best regards

    Erwan

    ________________

    Attachments :

    2015-04-10_102449.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qXVy&d=%2Fa%2F0X0000000bop%2Fe7xy8gZcB_Rsip6x7OFfXvfpLYJ8K6PLygUR.kk29Wk&asPdf=false

    2015-04-10_103017.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qXUb&d=%2Fa%2F0X0000000bon%2FaiFvvupOwNVn.8ylJDO_WaBCovxqevgkYLOnqKp27O8&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.