Skip to main content
Visitor II
Jul 21, 2025 12:51 PM UTC
Question

Unable to Connect SPC563M64 over JTAG Using UDESTK Programmer (UDE Software)

 

Hello,

I am trying to program the SPC563M64 microcontroller using the UDESTK programmer and UDE software.

Unfortunately, the JTAG interface cannot establish a connection with the MCU and I keep getting errors.

What I have tried so far:

  • Carefully checked all JTAG connections (TDI, TDO, TCK, TMS, TRST, and RESET).
  • Verified voltage levels on the board and programmer using a voltmeter and logic analyzer; signals look correct.
  • Tested the crystal oscillator with both 8MHz and 16MHz crystals to rule out clock issues.
  • Set the boot mode pins according to the datasheet.
  • Double-checked power and ground wiring; no issues found.

Current Problem:

Despite all these checks, the JTAG connection still fails and UDE gives errors such as “cannot identify device,” “flash not accessible,” or sometimes “CHK Fatal Error.”

If anyone has had a similar experience or can suggest a solution, I would really appreciate your help.

Thank you!

This topic has been closed for replies.