Skip to main content
fm_it
Associate
Aug 20, 2018 3:45 AM UTC
Question

UART Rx interrupt on SPC560D

SPC5 Studio for SPC560D-DIS board, LINFLEX0 configured as UART, Tx is okay but Rx ISR is not getting called. I am using the auto generated Serial Test application which creates IRQ handlers in "spc5_linflex.c". I have break points set in both Tx and Rx IRQ handlers, only Tx IRQ gets hit. I can see the RX data coming into BDRM buffer and UARTSR DRF (data receive flag) is also set. Please help.

    This topic has been closed for replies.

    1 reply

    procolo
    Visitor II
    Aug 29, 2018 8:47 AM UTC

    Hello,

    are you using spc5studio 5.8.1?

    If not please update your version of SPC5Studio to 5.8.1 and let us know if the problem still exist.

    Regards