Skip to main content
VNava.1
Associate III
Oct 21, 2021 7:40 AM UTC
Solved

There exist an example for SPC58EC-DISP that I can use in order to send UDP message from SPC58EC-DISP via Ethernet without include FreeRTOS Component?

Hi community!

my name is Vincenzo,

I am looking, if any, for an example application that would help me understand how to send UDP messages from the SPC58EC-DISP board over Ethernet.

For the moment I have found an interesting application that allows me to ping the SPC58EC-DISP from my PC, but I'm not being able to do anything else. I noticed that there are demos available inside this application such as Simple TCP Echo Server, but I have not been able to get it to work. There is some documentation about it? besides AN5413.

Moreover, I would like to know if it possible to create the Ethernet socket to send a UDP message without using the FreeRTOS Component RLA component?

Thanks in advance for your support!

Vincenzo

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Nov 22, 2021 4:27 PM UTC

    Hello ,

    There is no example for SPC58EC-DISP using Network component without FreeRTOS Component.

    These components are dependent on FreeRTOS.

    You need to recreate from scratch the Ethernet socket.

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Nov 22, 2021 4:27 PM UTC

    Hello ,

    There is no example for SPC58EC-DISP using Network component without FreeRTOS Component.

    These components are dependent on FreeRTOS.

    You need to recreate from scratch the Ethernet socket.

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.