The J‑Link Pro cannot establish a connection to SR6P3C4_HSM.
We are debugging with the J‑Link Pro PoE and have run into an issue: connection to SR6P3C4_HSM cannot be established, while CLUSTER_0_R52_0 attaches successfully. The device is a fresh SR6P3C4 MCU mounted on a PCBA. Please help investigate the possible causes and specify any special configurations needed to attach to the SR6P3C4_HSM core.
error infomations:
“
Application log started
- J-Flash V9.90 (J-Flash compiled Oct 28 2026 16:07:03)
- JLinkARM.dll V9.90 (DLL compiled Oct 28 2026 15:58:02)
Reading flash device list [C:\Program Files\SEGGER\JLink_V990\ETC/JFlash/Flash.csv] ...
- List of flash devices read successfully (451 Devices)
Reading MCU device list ...
- List of MCU devices read successfully (14814 Devices)
Creating new project ...
- New project created successfully
Connecting ...
- Connecting via USB to probe/ programmer device 0
- Probe/ Programmer firmware: J-Link Pro PoE V6 compiled Oct 21 2026 15:40:46
- Probe/ Programmer S/N: 1196000157
- Device "SR6P3C4_HSM" selected.
- Target interface speed: 50 kHz (Fixed)
- VTarget = 4.364V
- ConfigTargetSettings() start
- ConfigTargetSettings() end - Took 17us
- Found SW-DP with ID 0x4C013477
- Failed to power up DAP
- ConfigTargetSettings() start
- ConfigTargetSettings() end - Took 20us
- Found SW-DP with ID 0x4C013477
- Failed to power up DAP
- ERROR: Failed to connect.
Could not establish a connection to target.
General troubleshooting guide: https://kb.segger.com/J-Link_Troubleshooting
Device specific guide: https://kb.segger.com/ST_SR6P3
- ERROR: Connect failed “