Skip to main content
jmary
Associate III
Jul 31, 2023 1:35 AM UTC
Solved

Task on GTM DPLL loss lock callback in ECU?

Anyone here do ECU project with GTM on SPC57?

what task/function should I add on loss lock callback of the GTM DPLL? I saw some samples project, they switch to half cycle ( 360 degree ) on the loss lock callback event. but I still have no clue the benefit of this such task. perhaps anyone here have some suggestions.

This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Aug 28, 2023 3:25 PM UTC

There is a nice example in SPC5Studio

Have you checked this application ?

SPC572L64E3 ECU_ENGINE_LIB Test Application for Discovery

        Best regards

                        Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Aug 28, 2023 3:25 PM UTC

There is a nice example in SPC5Studio

Have you checked this application ?

SPC572L64E3 ECU_ENGINE_LIB Test Application for Discovery

        Best regards

                        Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
jmary
jmaryAuthor
Associate III
Sep 2, 2023 2:07 PM UTC

Yes, I had. The problem with the sample code there, after lost lock event the code then reinit the GTM. But then the pmt register became invalid.