Skip to main content
raghu tumati
Associate III
Sep 22, 2017 8:50 PM UTC
Question

sync PWMA0 and PWMA1

Posted on September 22, 2017 at 22:50

I have an application where I need to enable two PWM outputs. They need to have the same frequency but different duty cycles 

I have got PWMA0 and PWMA1 working but I am not able to get them synced together. There is a 9.2us difference in switching between A0 and A1. 

I tried playing around with the FORCE_EN register and but was unsuccessful. Is there any easy way to get this done?

    This topic has been closed for replies.

    6 replies

    Erwan YVIN
    ST Technical Moderator
    Sep 25, 2017 9:35 AM UTC
    Posted on September 25, 2017 at 11:35

    Hello Raghu ,

    Could you confirmed the device / microcontrollers used ? 

    Anyway , i am checking the FORCE_SEL register.

      Best regards

             Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    raghu tumati
    Associate III
    Sep 25, 2017 5:07 PM UTC
    Posted on September 25, 2017 at 17:07

    Hi Erwan 

    Thank you for replying. The micro is SPC560P50L5. Im using the SPC560P-DISP eval board. 

    I have used the following setting without much success. 

    For submodule0 

    INIT_SEL = 0

    RELOAD_SEL=0

    FORCE_SEL = 0

    FRCEN=1U

    For submodule1 

    INIT_SEL = 1U

    RELOAD_SEL =1U

    FORCE_SEL=1U

    FRCEN=1U

    And after that in the main.c file, I call 

    FORCE = 1 for submodule 0. I was hoping that a force on submodule 0 would cause the same in submodule 1 also from the register description in the data sheet. 

    But I think I'm missing something.

    raghu tumati
    Associate III
    Sep 25, 2017 8:08 PM UTC
    Posted on September 25, 2017 at 22:08

    Hi Erwan 

    I was able to get it working partially. 

    I commented the INIT_SEL and RELOAD_SEL and had just the FORCE_SEL and it worked. The two submodules are now synchronously switching only if their duty cycles are same.

    If their duty cycles are different, it does not work. Please see attached pictures. I have one of the submodules polarity inverted for the application. 

    0690X00000603yQQAQ.jpg0690X0000060470QAA.jpg
    raghu tumati
    Associate III
    Sep 26, 2017 12:11 AM UTC
    Posted on September 26, 2017 at 00:11

    Never mind. I figured this one out too. 

    The PWM was set to Align_Center and it should have been Align_Edge. 

    Sorry for the constant bombardment of replies in this thread. 

    Although Im still not done  

     I would like to switch a GPIO on and off multiple times from the rising edge of only one of the PWM submodules? What is the easiest way to do this? Timer or CTU or ICU? 

    -Raghu

    raghu tumati
    Associate III
    Oct 2, 2017 9:23 PM UTC
    Posted on October 02, 2017 at 21:23

    Hi Erwan

    I have this working now .Thanks for your help. 

    Erwan YVIN
    ST Technical Moderator
    Sep 26, 2017 8:31 AM UTC
    Posted on September 26, 2017 at 10:31

    Hello Raghu ,

    you are not far from the solution

    There is an example in the reference manual RM022

    Coudl you try to update INIT = VAL2 = VAL4 ?

    Chapter 26.7.2 Edge-aligned PWMs (INIT = VAL2 = VAL4)

    0690X00000608KZQAY.png

       Best Regards

                            Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.