Skip to main content
Visitor II
Aug 8, 2025 9:32 AM UTC
Question

supported debuggers & step-by-step procedure to flash SPC563M-DISP used with EVAL-L9945

Hi everyone  I’m stuck and would really appreciate guidance.

What I have,

Discovery board: SPC563M-DISP (the MCU on this board needs the L9945_GUIV1.0 ELF flashed).

EVK: EVAL-L9945 (L9945 MOSFET-driver evaluation board)  the L9945 evaluation package & GUI expect the discovery board MCU to be flashed with an ELF to run the demo

Questions.
1. How many/debugger types does SPC5 Studio support out of the box? Is PLS UDE the only officially supported debugger/plugin?

2. I have a PE MICRO Multilink  Can I use this to flash the SPC563M? If yes  what is the exact procedure (drivers, connection pins, which file formats are accepted: ELF / SREC / HEX)? 

3. If using UART/FLEXCAN flashing (serial boot), what exact steps  do you recommend? I’ve seen SPC5-Flasher mentioned  is that the tool to use for UART/CAN (which CAN like PCAN ,Vector) flashing?


 

Thanks & Regards,

Arif 

 

 

This topic has been closed for replies.