Skip to main content
Associate II
Apr 22, 2025 1:24 PM UTC
Question

suitable debugger for SPC560P ?

Moved from STM32 forum - SPC5 is not STM32


For the SPC560P50L5 microcontroller, I was using the SPC5Studio IDE. Can you suggest a suitable debugger?

This topic has been closed for replies.

5 replies

Andrew Neil
Super User
Apr 22, 2025 1:36 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Avinash_PAuthor
Associate II
Apr 23, 2025 5:22 AM UTC

Hi Andrew,

  Thanks for the immediate response. 

To understand the problem we are facing, let me break down the issue,

1. We have used ST LNK debugger which was obsolete now.

2. Now, to replace the debugger, we have bought AEK-MCU-SPC5LNK.

3. We are using SPC560P microcontroller. As it is mentioned in the datasheet, it can be used for the mentioned microcontroller.

4. We have downloaded AutoDevKit(Previously we are using SPC5Studio). and OpenOCD drivers as mentioned in the datasheet.

5. Now, while trying to debug the application, its asking for cfg file which was not available and SVD file  for SPC60P(not available).

Avinash_P_0-1745385656873.png

Kindly support us on this issue to use the new debugger.

 

 

Erwan YVIN
ST Technical Moderator
Apr 24, 2025 9:13 AM UTC

Hello ,

we do not support openocd for SPC56

i recommend to use on Windows

SPC5-UDESTK - USB/JTAG debugger for SPC5 MCUs with software license included (by PLS) - STMicroelectronics

Download SPC5-UDESTK

         Best regards

                      Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.