Skip to main content
Erwan YVIN
ST Technical Moderator
Feb 13, 2026 3:11 PM UTC
Solved

StellarStudio 9.0.0 officially pushed (Compliant for Java21 and eclipse 202512)

 

For your information, StellarStudio 9.0.0-LEDS has been finalized and pushed for the environments. (Windows, MacOS, Linux)

ezgif-84da9d196e6acb11.gif

This version is based on Eclipse 202512 and CDT 12.3.0, with standalone tools using Java 21.

  • StellarStudio Pinmap Configurator (SR5E1, SR6P3, SR6P3E, SR6P6, SR6P7G7 , SR6P7, SR6G7 and SR6G6)
  • StellarStudio Noc Configurator (SR6P7G7, SR6G6 , SR6P3 and SR6G7)
  • StellarStudio Clocktree Configurator (SR5E1, SR6P3, SR6P3E, SR6P6, SR6P7G7 , SR6P7, SR6G7 and SR6G6)
  • StellarStudio Power Conso Configurator (SR5E1 , SR6G6, SR6P7G7)

 

What's new in this release ?

StellarStudio 9.0.0-LEDS version is officially pushed. (Windows, MacOS, Linux) based on eclipse 202512 and the version CDT 12.3.0 with standalone tools (Java 21)

9.0.0 Common part:

  • Updated module versions
  • New starting Splash Screen

SR5E1 device

SR5E1 public device:

9.0.0 Initial part:

· Fixed "Is it possible to display the system clock?"

 

SR6 P and G devices

SR6 restricted devices (On demand, contact our sales office):

9.0.0 Initial part:

  • Integrated new Stellar SDK 5.2.1
  • Ported all SR6x demos to new Stellar SDK 5.2.1
  • New SR6x CAN GUI support
  • Fixed "SR6 clocktree red color not updated when CAN value is wrong"
  • Fixed "SR6 clocktree limit CAN clock to fixed frequencies"
  • Fixed "all SR6 devices should require CAN GUI"
  • Fixed "indexing do not work on imported SR6 demos"
  • Fixed "selecting one device, obtaining other demos"
  • Fixed "when selecting one device line, obtain other demos"
  • Fixed "SR6 AI console empty after analyze or generate"
  • Fixed "SR6 wrong CAN clock error message"
  • Fixed "SR6x limit FlexRay input to 80 MHz"
  • Fixed "Update of family filter when the filter product line is set to All lines in Application Wizard"
  • Fixed "Compile CAN canR52_Can2Can with default config"
  • Fixed "Compile PowerME meDrunSpStbyDrun_Automatic with default config"
  • Fixed "Compile CANXS canxs_Basic_Loopback with default config"
  • Fixed "Compile PowerME meDrunSpStbyDrun with default config"
  • Fixed "Compile PowerME meStop_Automatic with default config"

G6:

  • Fixed "Why is the programming time for StellarLink so long?"
  • Fixed "project name is not be listed after import as project"

P3:

  • Added SR6x CAN GUI Demo
  • Added NoC configuration support
  • Fixed "P3 AUX7 do not support PHI_LLC input"

P6:

  • Fixed "long to program a large elf file"

P3E:

  • Added P3E pinmap support
  • Added P3E clocktree support
  • Added new SR6P3EC6_saradcConversion demo
  • Added new SR6P3EC6_FreeRTOS_ping demo
  • Added new SR6P3EC6_canTxRx demo
  • Added new SR6P3EC6_canxsTxRx demo
  • Added new SR6P3EC6_multiLedBlink demo
  • Added new SR6P3EC6_K2000 demo
  • Fixed "P3E check CAN_XS clock is 160 MHz"
  • Fixed "P3E wrong colors in peripheral graph"

 

9.0.0 Known Limitations:

  • StellarLink probe does not support yet the debug of SR6P3E device
  • J-Link probe does not support yet the debug of SR6P3E device

 

9.0.0 Release Installation

  • Public update sites for SR5x

https://common.srxstudio.org/ (Core/Debug)

https://contrib.srxstudio.org/ (Motorcontrol / AI)

https://sr5.srxstudio.org/ (SR5x ESDK/Tools)

  • Restricted update sites for SR6x

https://sr6.srxstudio.org/ (SR6x SSDK/Tools) (secured update site for alpha customers)

  • Full/Light [Linux/MacOs] : is available on codex (on demand)
  • Update from StellarStudio 8.X.0 by using bookmarks-eclipse-202512.xml
  • image002.pngimage004.pngimage006.pngimage008.pngimage010.pngimage012.pngimage014.pngimage016.pngimage018.png
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Mar 9, 2026 2:59 PM UTC

Resources : StellarStudio | Software - STMicroelectronics

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Erwan YVIN
Erwan YVINAuthorBest answer
ST Technical Moderator
Mar 9, 2026 2:59 PM UTC
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.