Skip to main content
OHarc.1
Associate
Jul 12, 2023 10:49 AM UTC
Solved

Standard CAN Message with DLC > 8 using SPC5 LLD

Hello,

I know this is a bit of an edge case but during some testing today I noticed that the low level CAN drivers that come packaged with SPC5 studio only use the DLC field to work out how many bytes are in a recieved CAN the message. This isn't strictly correct as ISO 11898-1:2003 permits a standard CAN frame to have a DLC of > 8 which should be interpreted as a message containing the maximum 8 bytes. Unfortunately this ended up causing a hard-fault for me as the driver was trying to work on 64 bytes when only 8 had arrived. I have patched this locally by also checking the EDL bit when working out the frame size and thought this is something you may want to include in future.

Many thanks,
Owen 

This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Aug 29, 2023 12:33 PM UTC

Hello ,

These drivers are following the license SLA0098 http://download.spc5studio.com/updates/LICENSE.pdf

The CAN Drivers have been developed as example.

No problem to update it ;)

For yopur info , AUTOSAR MCAL (Microcontroller Abstraction Layer) CAN drivers are designed to follow the ISO 11898-1 standard.

                Best Regards

                             Erwan

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Aug 29, 2023 12:33 PM UTC

Hello ,

These drivers are following the license SLA0098 http://download.spc5studio.com/updates/LICENSE.pdf

The CAN Drivers have been developed as example.

No problem to update it ;)

For yopur info , AUTOSAR MCAL (Microcontroller Abstraction Layer) CAN drivers are designed to follow the ISO 11898-1 standard.

                Best Regards

                             Erwan

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.