Skip to main content
LMuel
Visitor II
Sep 20, 2021 10:17 AM UTC
Solved

ST SPC560C50L3C6E0X microntroller compatibility with NXP MPC5604CF2MLL6

Hi,

I'm currently checking for alternative for the MCU a that is part of a pcb we use. 0693W00000DniTHQAZ.pngFor the future, we want to store an alternative chip for all electronics. As far as I know, this is very easy for the automotive power pc SPC5 MCU because this IP has a variant of ST and NXP.

The question now is to what extent I can see how two chips are compatible in terms of function and pin layout.

In detail, it's about the two chips:

MPC5604CF2MLL6(of NXP) and SPC560C50L3C6E0X (of ST).

Thank you,

Regards.

Lars Mueller0693W00000DniSOQAZ.png

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Sep 29, 2021 2:40 PM UTC

    Hello ,

    you should download the different RM and compare the pin muxing.

    Anyway , it seems to be the same family.

    The IPs should be very similar ;)

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Sep 29, 2021 2:40 PM UTC

    Hello ,

    you should download the different RM and compare the pin muxing.

    Anyway , it seems to be the same family.

    The IPs should be very similar ;)

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.