Skip to main content
stefanodimascio9
Associate III
Dec 11, 2015 10:31 AM UTC
Question

SRAM faut injection

Posted on December 11, 2015 at 11:31

Hello everybody,

I'm working on the SPC56EL70L5

From the reference manual, I know that:

“For platform RAM, the intent is to generate errors during data write cycles, such that subsequent reads of the corrupted address locations generate ECC events, either single-bit corrections or double-bit non-correctable errors that are terminated with an error response.�?

So, I coded (I put the related assembly too):

SPP_MCM.ECR.R=0x33;  \\to activate reportings

0x00001D7E:   70 1F E7 F4  E_LIS     R0,0xFFF4

0x00001D82:   4B 37        SE_LI     R7,0x33

0x00001D84:   01 06        SE_MR     R6,R0

0x00001D86:   34 E6 00 43  E_STB     R7,0x43(R6)

SPP_MCM.EEGR.B.FR11BI=1;   \\ injection

0x00001D8A:   70 FF E7 F4  E_LIS     R7,0xFFF4

0x00001D8E:   50 07 00 48  E_LWZ     R0,0x48(R7)  

0x00001D92:   48 16        SE_LI     R6,0x1

0x00001D94:   74 C0 64 E6  E_RLWIMI  R0,R6,0xC,0x13,0x13

0x00001D98:   54 07 00 48  E_STW     R0,0x48(R7)

But, execution of instruction at 0x00001D8E causes hangs in

_unhandled_exception:0x000003A0:   78 00 00 00  E_B       _unhandled_exception (0x000003A0))

This is not the expected behavior, what is going wrong?

Thanks in advance for the help
    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Dec 14, 2015 2:45 PM UTC
    Posted on December 14, 2015 at 15:45

    Hello Stefano ,

    It is linked to the compiler optimization. to set a bitfield is not recommended in some compilers. I recommend to use the register directly :

    // Force RAM One 1-bit Data Inversion
    #define ECSM_EEGR_FR11BI_MASK 0x1000
     /* Force internal SRAM one 1-bit correctable data error */
     SPP_MCM.EEGR.R = (uint16_t)(ECSM_EEGR_FR11BI_MASK | 0); 

    Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    stefanodimascio9
    Associate III
    Dec 16, 2015 11:40 AM UTC
    Posted on December 16, 2015 at 12:40

    Thank you, it worked.

    Best Regards