[SR5E1E7] How to officially program DCF (C1_APPLI_ADDR_REG) for standalone Flash boot from BAF?
Hello ST Team and Community,
I am working with the SR5E1E7 MCU (Core 1 / Cortex-M7, evbe7000s board profile, StellarESDK-1.7.0, SR5E1_MCTK-1.3.0).
I have successfully flashed and verified my application binary into internal Flash at 0x08000000 using StellarLINK / OpenOCD. However, upon power-cycle or standalone reset, the CPU remains stuck in the BAF (Boot Assist Flash) (PC = 0x1FFxxxxx, VTOR = 0x1FF00100) instead of jumping to the application in Flash.
Current Register & Memory Observations:
-
Flash Vector Table (
0x08000000):0x24004798(valid initial MSP) -
Reset Vector (
0x08000004):0x08000401(validReset_Handler) -
C1_APPLI_ADDR_REG(0x4400030C):0x00000000(application address not yet registered) -
C1_VTOR_INIT_REG(0x44000304):0x1FF00100(currently pointing to BAF)
Current Workaround: When debugging via OpenOCD/GDB, manually overriding SP, PC, and VTOR allows the application (an LED blink test) to execute properly:
set $sp = 0x24004798
set $pc = 0x08000401
set *(unsigned int *)0xE000ED08 = 0x08000000
continue
Since RM0483 states that DCF records in the UTEST region (0x1FF80300) are non-reversible and limited to 4 updates, I have avoided writing to UTEST/DCF manually. Could you please provide the official ST tool, flash algorithm, or documented procedure/script to safely program the DCF record for C1_APPLI_ADDR_REG (0x08000000) so that Core 1 boots standalone from Flash?
Thank you!