Skip to main content
GMG
Associate III
Feb 27, 2022 4:33 PM UTC
Solved

SPC5x pinout

Hi, where can I find microcontroller pinout?

I miss something? I can't find spc5 pinouts in datasheets, where are these resources?

​

Best regards​

    This topic has been closed for replies.
    Giuseppe DI-GIORE
    ST Employee
    Feb 27, 2022 9:42 PM UTC

    Hello,

    for each SPC5 MCU pinout description is available in a specific technical note.

    See the MCU specific documentation page.

    For example, SPC58EC pinout is available in Technical Note TN1260 (link)

    Download the MCU specific I/O definition technical note, it is in pdf format,

    then the I/O pinout file is attached to the pdf as spreadsheet file.

    Regards.

    3 replies

    Giuseppe DI-GIORE
    ST Employee
    Feb 27, 2022 9:42 PM UTC

    Hello,

    for each SPC5 MCU pinout description is available in a specific technical note.

    See the MCU specific documentation page.

    For example, SPC58EC pinout is available in Technical Note TN1260 (link)

    Download the MCU specific I/O definition technical note, it is in pdf format,

    then the I/O pinout file is attached to the pdf as spreadsheet file.

    Regards.

    GMG
    GMGAuthor
    Associate III
    Feb 27, 2022 10:13 PM UTC

    thanks, opening the pdf from the browser it is not possible to see attachments and therefore I could not understand where they were.

    Giuseppe DI-GIORE
    ST Employee
    Feb 27, 2022 10:18 PM UTC

    Hello,

    please do not open the file in a browser, download it instead.

    Open with a pdf viewer, for example Acrobat Reader

    Open the left menu and click on the paperclip.

    0693W00000Kaim1QAB.pngRegards,