Skip to main content
Tim Tashpulatov
Associate
Nov 9, 2017 7:15 AM UTC
Solved

SPC5Studio: EMIOS register definitions for SPC56EC wrong?

Posted on November 09, 2017 at 08:15

I want to use EMIOS and PWM for SPC56EC74. When debugging the code for Channel 0, I can see that channel 9 is being initialized instead.

Looking into 

the xpc56ec.h file, EMIOS section, the UCDIS Disable Channel Register is being described starting at (Base+0x000F), whereas in the datasheet it is said to be at (Base+0x000C).

Is the xpc56ec.h header not compatible with SPC56EC74?

The code:

pwm_lld_init (); 

pwm_lld_start (&PWMD1, &pwm_config_pwmcfg);

pwm_lld_enable_channel (&PWMD1, 0, PWM_PERCENTAGE_TO_WIDTH(&PWMD1,5000));

The header in question is taken from the following plugin:

com.st.spc5.components.platform.spc56ecxx_rla_1.0.0.201707271939\component\lib\include\xpc56ec.h

Regards

Tim

#emios #spc56xx
    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Nov 9, 2017 9:00 AM UTC
    Posted on November 09, 2017 at 10:00

    Hello Tim ,

    ihave checkedthe header file

     union { /* Output Update Disable (Base+0x0008) */
     vuint32_t R;
     struct {
     vuint32_t OU31:1;
     vuint32_t OU30:1;
     vuint32_t OU29:1;
     vuint32_t OU28:1;
     vuint32_t OU27:1;
     vuint32_t OU26:1;
     vuint32_t OU25:1;
     vuint32_t OU24:1;
     vuint32_t OU23:1;
     vuint32_t OU22:1;
     vuint32_t OU21:1;
     vuint32_t OU20:1;
     vuint32_t OU19:1;
     vuint32_t OU18:1;
     vuint32_t OU17:1;
     vuint32_t OU16:1;
     vuint32_t OU15:1;
     vuint32_t OU14:1;
     vuint32_t OU13:1;
     vuint32_t OU12:1;
     vuint32_t OU11:1;
     vuint32_t OU10:1;
     vuint32_t OU9:1;
     vuint32_t OU8:1;
     vuint32_t OU7:1;
     vuint32_t OU6:1;
     vuint32_t OU5:1;
     vuint32_t OU4:1;
     vuint32_t OU3:1;
     vuint32_t OU2:1;
     vuint32_t OU1:1;
     vuint32_t OU0:1;
     } B;
     } OUDR;
     union { /* Disable Channel (Base+0x000F) */
     vuint32_t R;
     struct {
     vuint32_t CHDIS31:1;
     vuint32_t CHDIS30:1;
     vuint32_t CHDIS29:1;
     vuint32_t CHDIS28:1;
     vuint32_t CHDIS27:1;
     vuint32_t CHDIS26:1;
     vuint32_t CHDIS25:1;
     vuint32_t CHDIS24:1;
     vuint32_t CHDIS23:1;
     vuint32_t CHDIS22:1;
     vuint32_t CHDIS21:1;
     vuint32_t CHDIS20:1;
     vuint32_t CHDIS19:1;
     vuint32_t CHDIS18:1;
     vuint32_t CHDIS17:1;
     vuint32_t CHDIS16:1;
     vuint32_t CHDIS15:1;
     vuint32_t CHDIS14:1;
     vuint32_t CHDIS13:1;
     vuint32_t CHDIS12:1;
     vuint32_t CHDIS11:1;
     vuint32_t CHDIS10:1;
     vuint32_t CHDIS9:1;
     vuint32_t CHDIS8:1;
     vuint32_t CHDIS7:1;
     vuint32_t CHDIS6:1;
     vuint32_t CHDIS5:1;
     vuint32_t CHDIS4:1;
     vuint32_t CHDIS3:1;
     vuint32_t CHDIS2:1;
     vuint32_t CHDIS1:1;
     vuint32_t CHDIS0:1;
     } B;
     } UCDIS;�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    The comments are false

    it should not be :

    /* Disable Channel (Base+0x000F) */�?

    it should be 0x8 +x04 = 0xC

    /* Disable Channel (Base+0x000C) */�?

    i am creating an ER to correct the header file and to integrate it in the last components version

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Nov 9, 2017 9:00 AM UTC
    Posted on November 09, 2017 at 10:00

    Hello Tim ,

    ihave checkedthe header file

     union { /* Output Update Disable (Base+0x0008) */
     vuint32_t R;
     struct {
     vuint32_t OU31:1;
     vuint32_t OU30:1;
     vuint32_t OU29:1;
     vuint32_t OU28:1;
     vuint32_t OU27:1;
     vuint32_t OU26:1;
     vuint32_t OU25:1;
     vuint32_t OU24:1;
     vuint32_t OU23:1;
     vuint32_t OU22:1;
     vuint32_t OU21:1;
     vuint32_t OU20:1;
     vuint32_t OU19:1;
     vuint32_t OU18:1;
     vuint32_t OU17:1;
     vuint32_t OU16:1;
     vuint32_t OU15:1;
     vuint32_t OU14:1;
     vuint32_t OU13:1;
     vuint32_t OU12:1;
     vuint32_t OU11:1;
     vuint32_t OU10:1;
     vuint32_t OU9:1;
     vuint32_t OU8:1;
     vuint32_t OU7:1;
     vuint32_t OU6:1;
     vuint32_t OU5:1;
     vuint32_t OU4:1;
     vuint32_t OU3:1;
     vuint32_t OU2:1;
     vuint32_t OU1:1;
     vuint32_t OU0:1;
     } B;
     } OUDR;
     union { /* Disable Channel (Base+0x000F) */
     vuint32_t R;
     struct {
     vuint32_t CHDIS31:1;
     vuint32_t CHDIS30:1;
     vuint32_t CHDIS29:1;
     vuint32_t CHDIS28:1;
     vuint32_t CHDIS27:1;
     vuint32_t CHDIS26:1;
     vuint32_t CHDIS25:1;
     vuint32_t CHDIS24:1;
     vuint32_t CHDIS23:1;
     vuint32_t CHDIS22:1;
     vuint32_t CHDIS21:1;
     vuint32_t CHDIS20:1;
     vuint32_t CHDIS19:1;
     vuint32_t CHDIS18:1;
     vuint32_t CHDIS17:1;
     vuint32_t CHDIS16:1;
     vuint32_t CHDIS15:1;
     vuint32_t CHDIS14:1;
     vuint32_t CHDIS13:1;
     vuint32_t CHDIS12:1;
     vuint32_t CHDIS11:1;
     vuint32_t CHDIS10:1;
     vuint32_t CHDIS9:1;
     vuint32_t CHDIS8:1;
     vuint32_t CHDIS7:1;
     vuint32_t CHDIS6:1;
     vuint32_t CHDIS5:1;
     vuint32_t CHDIS4:1;
     vuint32_t CHDIS3:1;
     vuint32_t CHDIS2:1;
     vuint32_t CHDIS1:1;
     vuint32_t CHDIS0:1;
     } B;
     } UCDIS;�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    The comments are false

    it should not be :

    /* Disable Channel (Base+0x000F) */�?

    it should be 0x8 +x04 = 0xC

    /* Disable Channel (Base+0x000C) */�?

    i am creating an ER to correct the header file and to integrate it in the last components version

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Tim Tashpulatov
    Associate
    Nov 9, 2017 11:08 AM UTC
    Posted on November 09, 2017 at 11:08

    Hello Erwan,

    Thank you for prompt reply. Indeed, it seems to be the comments issue, as the code is working as it should. I yet have to understand the reason behind EMIOS group 0 using channels starting from 9 and up, but this may be the way PWM LLD works.

    Regards

    Tim