Skip to main content
QPATR
Associate
Nov 2, 2020 12:19 PM UTC
Solved

SPC5Studio 5.8.1 pin map editor bug

Hello, pin map editor is buggy for pins 88/89 of SPC564A80L7 and set always these pins as CAN and not eSCI when the pin map editor is opened and closed, code is generated as CAN!

I have modified thse pins function then directly in the code.

Thanks for your attention,

Best regards.

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Nov 2, 2020 1:55 PM UTC

    Hello ,

    generated code is in board.c

    No issue happened on SPC5Studio 5.8.1+ and 6.0

     {(int32_t)PCR_INDEX(PORT5, PIN_CAN_B_TX), PAL_LOW, (iomode_t)(PAL_MODE_OUTPUT_ALTERNATE_PRIMARY)},
     {(int32_t)PCR_INDEX(PORT5, PIN_CAN_B_RX), PAL_LOW, (iomode_t)(PAL_MODE_INPUT_ALTERNATE_PRIMARY)},
     
     {(int32_t)PCR_INDEX(PORT5, PIN_SCI_C_TX), PAL_LOW, (iomode_t)(PAL_MODE_OUTPUT_ALTERNATE(2))},
     {(int32_t)PCR_INDEX(PORT5, PIN_SCI_C_RX), PAL_LOW, (iomode_t)(PAL_MODE_INPUT_ALTERNATE(2))},

    Do not forget to save the configuration editor after saving and closing the pinmap editor ?

    Could you send me your installation details ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Nov 2, 2020 1:55 PM UTC

    Hello ,

    generated code is in board.c

    No issue happened on SPC5Studio 5.8.1+ and 6.0

     {(int32_t)PCR_INDEX(PORT5, PIN_CAN_B_TX), PAL_LOW, (iomode_t)(PAL_MODE_OUTPUT_ALTERNATE_PRIMARY)},
     {(int32_t)PCR_INDEX(PORT5, PIN_CAN_B_RX), PAL_LOW, (iomode_t)(PAL_MODE_INPUT_ALTERNATE_PRIMARY)},
     
     {(int32_t)PCR_INDEX(PORT5, PIN_SCI_C_TX), PAL_LOW, (iomode_t)(PAL_MODE_OUTPUT_ALTERNATE(2))},
     {(int32_t)PCR_INDEX(PORT5, PIN_SCI_C_RX), PAL_LOW, (iomode_t)(PAL_MODE_INPUT_ALTERNATE(2))},

    Do not forget to save the configuration editor after saving and closing the pinmap editor ?

    Could you send me your installation details ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.