Skip to main content
PParf.1
Associate
Mar 21, 2020 1:11 PM UTC
Solved

SPC5Studio 5.8.1 instalation - not found make.exe

New installation from scratch of SPCStudio 5.8.1 gives error that make is not found. I start a project with GCC and cant build the project. I cant find the make.exe nowhere except the hightec plugin folders.

When I add those folders i got other errors like

"make -j12 all 

System nie moľe odnale«† okre?lonej ?cieľki.

The syntax of the command is incorrect.

make: *** [build] Error 1

components/spc560dxx_platform_component_rla/lib/rsc/rules.mk:117: recipe for target 'build' failed"

My Path is C:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.hightec.win32_1.0.0.201809141314\hightec\ppc-ht-eabi\bin;C:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.hightec.win32_1.0.0.201809141314\hightec\bin;C:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20190604105544\toolchain\bin;C:\SPC5Studio\eclipse\configuration\org.eclipse.osgi\669\0\.cp\gnutools;

Also the folder included normally in path "C:\SPC5Studio\eclipse\configuration\org.eclipse.osgi\669\0\.cp\gnutools" does not exist.

How to solve this issue?

If here is solution to this problem... How to search for it? The search engine is total massacre...

Where to download EARLIER software releases than 5.8.1 which does not work ?

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Mar 31, 2020 1:08 PM UTC

    Hello ,

    1) Could you send me your installation details (Help ==> About SPC5Studio) ?

    2) Could you send me .metadata/.log located ion your workspace directory ?

    Just a note , it is important to update SPC5Studio in the new version

    http://download.spc5studio.com/updates/

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    6 replies

    Erwan YVIN
    ST Technical Moderator
    Mar 30, 2020 2:05 PM UTC

    hello ,

    Makefile used is in a Internal SPC5Studio Plugins

    it is automatically imported in the PATH

    it should be located

    c:\SPC5Studio\eclipse\configuration\org.eclipse.osgi\XXXX\X\.cp\gnutools\

    Could you send me your installation details ?

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    CFANG.2
    Visitor II
    Mar 31, 2020 9:11 AM UTC

    Yes, I have got the same problem.

    Just use the attached files from ST technical support, copy it into the directory "c:\SPC5Studio\eclipse\configuration\org.eclipse.osgi\" and add the path into the system path.

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Mar 31, 2020 1:08 PM UTC

    Hello ,

    1) Could you send me your installation details (Help ==> About SPC5Studio) ?

    2) Could you send me .metadata/.log located ion your workspace directory ?

    Just a note , it is important to update SPC5Studio in the new version

    http://download.spc5studio.com/updates/

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    CFANG.2
    Visitor II
    Mar 31, 2020 4:40 PM UTC

    Dear Erwan,

    I think I got almost the latest version, :)

    And I tested two version of SPC5Studio 5.8.1 from local ST support engineer and encounted the same problem.

    I have attached the two files you requested.

    By the way, do you have some informatoin about the PinMAP support for SPC58NH(cut2, LQFP176)?

    Because now I can select only FBPGA386 in SPC5Studio.

    Thank you for your help.

    Regards,

    Cheng FANG

    ​