Skip to main content
Erwan YVIN
ST Technical Moderator
Jan 26, 2015 3:57 PM UTC
Question

SPC5STudio 3.4.0 is available !

Posted on January 26, 2015 at 16:57

SPC5STudio 3.4.0 is available !

Dear Users,

The 3.4.0 release is now available on the update site.

Here are is the change log

SPC5STUDIO CORE :

- Patch mode: newly created project is already patched

- Implementing invisible groups

- Allow user to patch components/lib/ files: V2

- Patch mode : patch.xml to be hidden / Default / Grey Decorators

- Implement Hidden properties

SPC5STUDIO Repository :

- Create NIL RTOS SPC560Bxx Test Application for Discovery

SPC5STUDIO Pinmap :

- Unable to Set more than 10 pin in PinMap Wizard

SPC5-HAL :

- CAN Naming convention : Change the id number of Filter Settings

- The message buffers Tx/Rx Configuration in CAN module are fixed

- The incorrect registers bits definitions and driver data structures and types in hal_lld.h head file

- eMIOS channels 1,3,5,6,2,4,11,13 are not usable for ICU

- PWM/ICU functions on eMIOS

NIL RTOS :

- New feature for SPC560Bxx

We wish you a happy usage.

The SPC5Studio team.

#latest-release
    This topic has been closed for replies.

    5 replies

    ssk
    Associate III
    Jan 28, 2015 2:05 PM UTC
    Posted on January 28, 2015 at 15:05

    Hello Erwan,

    From where can I download the latest release? I tried from 'spc5.drive.cloudforge.com/projects/spc5releases/' but I am not finding it here.

    What is the update site?

    Please help. Thanks in advance.

    Mike.

    Erwan YVIN
    ST Technical Moderator
    Jan 30, 2015 10:06 AM UTC
    Posted on January 30, 2015 at 11:06

    Hello Mike ,

    You have to use the menu :

    Help ==> Install New software

    and pick on SPC5Studio Update site

    do not forget to put your proxy settings in Windows ==> Preferences (Network)

                    Best Regards

                                 Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ssk
    Associate III
    Jan 30, 2015 11:02 AM UTC
    Posted on January 30, 2015 at 12:02

    Hello Erwan,

    How to download in case the PC is not having the internet connection? I am using SPC5Studio on a lab PC where internet connection is not available.

    Thanks.

    Mike.
    Erwan YVIN
    ST Technical Moderator
    Feb 6, 2015 2:25 PM UTC
    Posted on February 06, 2015 at 15:25

    Hello Mike ,

    in the next days , we will send you a direct link to download the patch by ZIP File

    Best regards

                    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ssk
    Associate III
    Feb 9, 2015 5:57 AM UTC
    Posted on February 09, 2015 at 06:57

    Thanks Erwan. I am eagerly waiting for the link!! Look forward to receive it at the earliest.

    Thanks.

    Mike.