Skip to main content
HNguy.20
Associate
Jan 11, 2022 7:27 AM UTC
Solved

SPC58xHx BAF code loops in infinitely after reset or re-powered

Dear Experts,

After erasing all flash, I flash new program to SPC58 and it can just work as soon as flashing the application execution file (e.g. elf).

My SPC58 cannot run the application code after reset or re-powered.

Based on the SPC58 H Line Reference Manual, I checked the Boot record structure searched by the BAF on SPC58 flash and they all was correct as I've known:

  • Addr 0x00FC_0000: value=0x00A50000
  • Addr 0x00FC_0004: value=0x00FC8000 (It is start address of Boot CPU (Core2) Reset vector table)

0693W00000HrBs3QAF.pngI think I missing any setting for SPC58 flash but I cannot find more information currently.

So please help me if you was experienced about this.

Thanks in advance!

Ben

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jan 11, 2022 3:03 PM UTC

    Hello ,

    If you erase all the flash, you can not run your application.

    the strategy to detect a valid boot header is detailed in the figure 47.

    Your address seems to be correct :

    Please enter to debug session with your debugger

    your reset address should be 0xFC0008

    0693W00000HrGUuQAN.png Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jan 11, 2022 3:03 PM UTC

    Hello ,

    If you erase all the flash, you can not run your application.

    the strategy to detect a valid boot header is detailed in the figure 47.

    Your address seems to be correct :

    Please enter to debug session with your debugger

    your reset address should be 0xFC0008

    0693W00000HrGUuQAN.png Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    HNguy.20
    HNguy.20Author
    Associate
    Jan 12, 2022 2:06 AM UTC

    Hello Erwan,

    Thank you so much for your support.

    I'll try according to your advice.