Skip to main content
CoolMo
Associate II
Feb 22, 2022 10:01 AM UTC
Question

[SPC58Nxx] GTM 344 and TOMs granuliarity?

Hallo Everyone,

If I setup two TOM channels with the TOM module clocked at 100MHz: (10nSec)

  • GTM clocked at 100MHz
  • CMD.CFGU.EN_CLK0 = true
  • CMD.CFGU.CLK_DIV0 = 1
  • TOM0 module enabled
  • TOM0_4 source clock = CMU_FXCLK0
  • TOM0_4 period = 10000
  • TOM0_4 duty = 5000
  • TOM0_3 source clock = CMU_FXCLK0
  • TOM0_3 period = 10000
  • TOM0_3 duty = 4800

[EDIT]

Use an oscilloscope with sufficient speed and sampling buffer.

I was using a rough tool which was not allowing me to see into deep.

    This topic has been closed for replies.

    2 replies

    CoolMo
    CoolMoAuthor
    Associate II
    Feb 22, 2022 10:29 AM UTC

    btw: the code to verify this is trivial:

    int main(void) {

     const uint32_t period = 10000U;

     uint32_t duty_tom3 = 4200U;

     uint32_t duty_tom4 = 5000U;

     /* Initialization of all the imported components in the order specified in

       the application wizard. The function is generated automatically.*/

     componentsInit();

     /* Uncomment the below routine to Enable Interrupts. */

     /* irqIsrEnable(); */

     GTM_TOMDriver *pTom = &TOMD1;

     gtm_tomSetCompareReg1(pTom, TOM_CHANNEL3, period);

     gtm_tomSetCompareReg2(pTom, TOM_CHANNEL3, duty_tom3);

     gtm_tomSetCompareReg1(pTom, TOM_CHANNEL4, period);

     gtm_tomSetCompareReg2(pTom, TOM_CHANNEL4, duty_tom4);

     //simultaneous TOMs start

     gtm_tomStart();

     //start the Clock Management Unit (which generates fixed clocks for TOMs)

     gtm_cmuStart(&CMUD1);

     /* Application main loop.*/

     for ( ; ; ) {

     //do nothing

     }

    }

    ECAST.1
    Visitor II
    Feb 23, 2022 1:59 PM UTC

    Hello,

    I've used your code in a SPC5Studio project for Bernina MCU, and the correct value of Duty and Period are triggered.0693W00000KaFpaQAF.jpg 

    Come back to the original issue...

    The TOM0_4 starts with settings period = 10000 and duty= 5000

    The TOM0_3 starts with settings period = 10000 and duty= 4800

    After 5 seconds (running) the duty of TOM0_3 is updated to 4600 using the API

    gtm_tomUpdate_Duty_sync(&TOMD1, TOM_CHANNEL3, 4600);

    (this API call the low level function gtm_tomSetCompareReg2())

    Also in this case correct value are triggered.

    0693W00000KaFvTQAV.jpg 

    If you are using the SPC5Studio in the attachment the project used.

    Please focus in the GTM component configuration.

    Regards,

    Emanuele