Skip to main content
sonerb
Associate
Dec 14, 2022 9:55 AM UTC
Question

SPC58EN84C3 ADC test channel initialize error.

I tried to initialize test channels on SARADC_B (supervisor).

/* Channels Configurations (DMA is not used)*/
static channelConfig _saradcconf_ch_configs[SPC5_SARADC_MAX_NUMOFCHANNELS] =
{
 {SARADC_CHANNEL_TEST, 96U,SARADC_REFERENCE_DEFAULT, SARADC_PRECHARGE_ENABLED, SARADC_CTR0, SARADC_WATCHDOG_REGISTER_NONE,NULL},
 {SARADC_CHANNEL_TEST, 97U,SARADC_REFERENCE_DEFAULT, SARADC_PRECHARGE_ENABLED, SARADC_CTR0, SARADC_WATCHDOG_REGISTER_NONE,NULL},
 {SARADC_CHANNEL_TEST, 98U,SARADC_REFERENCE_DEFAULT, SARADC_PRECHARGE_ENABLED, SARADC_CTR0, SARADC_WATCHDOG_REGISTER_NONE,NULL},
 {SARADC_CHANNEL_TEST, 99U,SARADC_REFERENCE_DEFAULT, SARADC_PRECHARGE_ENABLED, SARADC_CTR0, SARADC_WATCHDOG_REGISTER_NONE,NULL},
 {0U, 0U, 0U, 0U, 0U, 0xFFU, NULL}, /* Channel Configuration Unused 4 */
 {0U, 0U, 0U, 0U, 0U, 0xFFU, NULL}, /* Channel Configuration Unused 5 */
};
 
 
/**
 * @brief Structure defining the configuration "saradcconf".
 */
SARADCConfig saradc_config_saradcconf = {
 /* conversion mode */
 SARADC_MODE_ONESHOT,
 
 /* Trigger Mode */
 SARADC_TRIGGER_DISABLED,
 
 /* CTR registers configuration (CRES,PRECHG,INPSAMP) */
 {
 /* CTR0 */ {SARADC_CRES_HIGH, 1U, 100U},
 /* CTR1 */ {SARADC_CRES_HIGH, 1U, 100U},
 /* CTR2 */ {SARADC_CRES_HIGH, 1U, 100U},
 /* CTR3 */ {SARADC_CRES_HIGH, 1U, 100U},
 },
 /* No DMA configuration */
 FALSE,
 {0U, 0U, 0U, 0U, 0U, 0U, 0U},
 NULL,
 
 /* Channels Configurations */
 _saradcconf_ch_configs,
 
 /* Number of channels */
 4U,
 
 /* Conversion callback */
 saradcconf_conv_cb,
 
 /* No analog watchdog configured */
 {
 {(float)0,(float)0},
 },
 (float)0,
 0U,
};

saradc_lld_start(&SARADC12DSV, &saradc_config_saradcconf);

While debugging I realized it goes to '.unhandled_exception2' when I tried to set TCDR[x].B.PCE (precharge bit.)

I tried to set all precharge disabled and enabled, but it still not working.

Here are some screenshots from debug view.

0693W00000WKz9qQAD.png0693W00000WKz4cQAD.png0693W00000WKz9CQAT.png0693W00000WKz92QAD.png 

This topic has been closed for replies.

2 replies

Erwan YVIN
ST Technical Moderator
Dec 14, 2022 1:18 PM UTC

Hello ,

Which compiler do you use ?

Could you try to compile this part of code in -O0 ?

Best Regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
sonerb
sonerbAuthor
Associate
Dec 14, 2022 1:46 PM UTC

0693W00000WL0ViQAL.pngI use FreeGCC.

I already built with -O0