Skip to main content
Explorer
Apr 19, 2024 3:30 PM UTC
Solved

SPC58ECxx C++ std::string throws linker errors

I'm working on a state machine for a console application, and I would like to use std::strings in C++, as they are much nicer to work with than C-style strings.

Including the string library does not result in errors, but when I call string objects in the code I start to get errors.  Here's an example of the code I am using:

//const char* output;		//No errors in c-style strings
std::string(output);		//Compiles, but results in linker error
switch(mState)
{
	case MAIN_STATE:
		output = "\r\nmain->";
		break;
	case CAN_STATE:
		output = "\r\ncan->";
		break;
	case UART_STATE:
		output = "\r\nuart->";
		break;
	case GPIO_STATE:
		output = "\r\ngpio->";
		break;
	default:
		output = "\r\nMAIN->";
		break;
}
//Print(output);	//No errors with C-style Strings
Print(output.c_str());	//Compiles, but results in linker error

 As I indicated in the code comments, any time I call a function from the <string> library, I get the following linker error:

07:41:57 **** Incremental Build of configuration Default for project ConsoleApp ****
make -j28 all 
Compiling cConsole.cpp
Linking build/out.elf
c:/spc5studio-6.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514/toolchain/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle/lib/e200z4\libc.a(lib_a-abort.o): 
In function `abort':
abort.c:(.text.abort+0x10): undefined reference to `_exit'
c:/spc5studio-6.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514/toolchain/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle/lib/e200z4\libc.a(lib_a-sbrkr.o): 
In function `_sbrk_r':
sbrkr.c:(.text._sbrk_r+0x1a): undefined reference to `sbrk'
c:/spc5studio-6.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514/toolchain/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle/lib/e200z4\libc.a(lib_a-signalr.o): 
In function `_kill_r':
signalr.c:(.text._kill_r+0x1c): undefined reference to `kill'
c:/spc5studio-6.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514/toolchain/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle/lib/e200z4\libc.a(lib_a-signalr.o): 
In function `_getpid_r':
signalr.c:(.text._getpid_r+0x0): undefined reference to `getpid'
collect2.exe: error: ld returned 1 exit status
make: *** [components/spc58ecxx_platform_component_rla/lib/rsc/rules.mk:164: build/out.elf] Error 1
"make -j28 all" terminated with exit code 2. Build might be incomplete.

07:42:06 Build Failed. 5 errors, 0 warnings. (took 9s.6ms)

 Interestingly, I've also noticed these kinds of errors with other standard C++ Libraries like <array> or <vector>.

These are my current linker settings:

Screenshot 2024-04-19 092256.png

 

 

 

 

 

 

 

 

What do I need to change in my linker settings to get the standard C++ libraries to link/build correctly?

This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Apr 24, 2024 8:01 AM UTC

Yes, it is possible but it is not so easy 

i recommend to follow to create the missing function in your project

Solved: SPC5Studio cannot use the malloc() and free() func... - STMicroelectronics Community

                 Best Regards

                                            Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Apr 24, 2024 8:01 AM UTC

Yes, it is possible but it is not so easy 

i recommend to follow to create the missing function in your project

Solved: SPC5Studio cannot use the malloc() and free() func... - STMicroelectronics Community

                 Best Regards

                                            Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.