Skip to main content
Yali Mobilities
Associate III
Jun 19, 2024 1:26 PM UTC
Solved

SPC58EC80 CanBus RTR Frame Request

I'm using SPC58 DISP Board for RTR request data frame from a battery pack. I have set the RTR value as 1, but didn't receive any reponse data frame from the battery. I have tested with CAN analyser, reponse data frame is coming(working fine). When I looked into the code, I didn't see any RTR register loading with the value. So, if anyone worked on RTR frame request. Kindly guide me.

Screenshot 2024-06-19 185331.png

Transmit data frame with RTR as 1.

 

This topic has been closed for replies.
Yali Mobilities
Yali MobilitiesBest answer
Associate III
Jul 18, 2024 12:11 PM UTC

Hi,

Actually I'm using CAN2.0 without FD.

I got RTR frame by adding some code which is included below. But the problem is If I tried change the data, its doesn't change in the CANbus message.

The code I included before the "Data Length" section in the "can_lld_writeTxBuffer" function.Screenshot 2024-07-18 172639.png

The code in the main function. Here I have increamented the data8[0] by 1 every loop. But it doesn't reflect in the CANbus message.Screenshot 2024-07-18 172055.png

Screenshot 2024-07-18 173640.png

The edited "can_lld.c" file is attached.

Best regards

Sharan

2 replies

Erwan YVIN
ST Technical Moderator
Jul 16, 2024 7:42 AM UTC

Hello ,

do you solve your issue ?

Are you well in CAN FD Format ?

ErwanYVIN_0-1721115640236.png

          Best Regards

                       Erwan

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Yali Mobilities
Yali MobilitiesAuthorBest answer
Associate III
Jul 18, 2024 12:11 PM UTC

Hi,

Actually I'm using CAN2.0 without FD.

I got RTR frame by adding some code which is included below. But the problem is If I tried change the data, its doesn't change in the CANbus message.

The code I included before the "Data Length" section in the "can_lld_writeTxBuffer" function.Screenshot 2024-07-18 172639.png

The code in the main function. Here I have increamented the data8[0] by 1 every loop. But it doesn't reflect in the CANbus message.Screenshot 2024-07-18 172055.png

Screenshot 2024-07-18 173640.png

The edited "can_lld.c" file is attached.

Best regards

Sharan